23.1.1 The
Options
dialog (for program-wide options)
Note
This section refers to the
Options
command on the main menu bar.
23.1.1.1
Recording
tab
File name prefix
: The prefix that will be inserted in file names for recordings.
Image format
: The image format for snapshots that are saved as image files from recordings.
Video format
: The video format for recordings.
Browse
: Click
Browse
to specify the location where video recordings will be saved.
Disk space
: The available disk space for recordings.
23.1.1.2
View
tab
Hide cold and hot spot
: To hide any existing cold and hot spots in an image, select this check box.
Show wizard when connecting a camera
: To display the import guide when connecting a camera, select this checkbox.
Use entire-scale setting on auto-adjust image
: (Applies to FLIR GF3xx cameras only.) To use the image’s entire temperature range when importing the image into FLIR Tools/Tools+, and not only the scene temperature range, select this check box. If this check box is not selected, the image may appear
considerably darker after importing, since FLIR Tools/Tools+ uses a default temperature range. For more information about the scene temperature range, see the FLIR GF3xx camera manual.
23.1.1.3
Library
tab
Add existing folder to library
: To add an existing folder on your computer to the image library, click
Browse
and navigate to the folder.
Remove folder
: To remove a folder from the image library, select the folder in the folder list and then click
Remove folder
.
23.1.1.4
Report
tab
Page size
: To change the page size, select a new page size in the list. Available options are
A4
,
US Letter
, and
US Legal
.
Show all parameters
: To display all measurement parameters for an image when included in a report, select this checkbox.
Extract digital camera image from thermal image (if available) when generating
: For cameras supporting multispectral images, all image modes are included inside a single image file—MSX, thermal, thermal
fusion, thermal blending, picture-in-picture, and the digital camera image. To extract the digital camera image when generating
a report, select this checkbox.
User Report Studio templates path
: The file path to the program’s Report Studio templates (Microsoft Word *.dotx files).
Logo
: To display a logo in the top left corner of the report pages, select this checkbox. To display another logo, click
Browse
and navigate to the logo file.
Header
: A text field where you can enter any text that shall be displayed in the report header.
Footer
: A text field where you can enter any text that shall be displayed in the report footer.
23.1.1.5
Units
tab
Temperature unit
: The unit for temperature values in the program and the reports. To change the unit, select another unit. Available options
are
Celsius
,
Fahrenheit
,
Kelvin
.
Distance unit
: The unit for distance in the program and the reports. To change the unit, select another unit. Available options are
Meters
,
Feet
.
23.1.1.6
Language
tab
Language
: To change the language, select a new language in the list.
23.1.2 The
Options
dialog (for plot-specific options)
Note
This section refers to the
Options
command on the main menu bar.
Chart title
: To change the title of the plot, type a title here.
Number of points
: Number of sampling points that the plot is based on.
Show cross-hairs
: To display a cross-hair that moves when you move the mouse and displays the X and Y axes values, select this checkbox.
Show latest value
: To display the latest Y value, select this checkbox.
X axis
>
Auto
: To let FLIR Tools/Tools+ automatically set the boundaries of the X axis, select
Auto
.
X axis
>
Manual
: To manually set the boundaries of the X axis, select
Manual
and enter the start and stop times.
Y axis
>
Auto
: To let FLIR Tools/Tools+ automatically set the boundaries of the Y axis, select
Auto
.
Y axis
>
Manual
: To manually set the boundaries of the Y axis, select
Manual
and enter the min. and max. values.