17  Creating reports

17.1   General

You can create the following types of reports from the program:

17.2  Setting a default report template

Prior to working with reports, you need to set a default report template. A maximum of two default report templates can be set. These templates will then be used when clicking Generate report on the Library tab.

17.3  Saving a report in the intermediary *.repx format

17.4  Creating an Adobe PDF imagesheet

17.5  Creating an Adobe PDF report

17.6  Creating a radiometric Microsoft Word‎ report