Follow this procedure:
Start the FLIR Report Studio wizard by doing one of the following:
In the left pane, select All Templates to display all of the templates available in FLIR Report Studio or select a template category to locate a particular report template.
In the center pane, click a report template. A preview of each page in the selected report template will be displayed in the right pane.
To continue with the selected template, click Next at the bottom of the window.

In the left pane, choose the folder containing the images to include in the report. You can also import images from a camera connected to the computer, by clicking Import at the left bottom of the window.

To add images to the report, do one or more of the following:

In the right pane, you can do the following:
To edit an image, do one of the following:
This opens the FLIR Report Studio Image Editor. For more information, see section 19 Analyzing and editing images using the FLIR Report Studio Image Editor .
Enter the name of the report in the REPORT NAME field in the upper part of the window.
Click the Generate arrow at the bottom of the window. Select one of the following:

The Report Properties dialog box is displayed.
Do one or more of the following:
To create the report with the displayed properties, click OK. This generates a report saved to the reports folder, as specified in Settings. For more information, see section 21.5 Changing the settings .
The report opens as a Microsoft Word document. The selected image(s) and the information entered in the Report Properties dialog box populate the corresponding placeholders in the report.
(Applicable to editable reports.) To edit an image, do one of the following:
This opens the FLIR Report Studio Image Editor. For more information, see section 19 Analyzing and editing images using the FLIR Report Studio Image Editor .
(Applicable to editable reports.) To modify objects in the report, refer to section 18.2 Managing objects in the report .
Save the report.
Follow this procedure:
Select Options > Settings.
In the Report tab, you can select settings related to the creation of reports.
In the Units tab, you can select settings related to temperature and distance units.
In the Import tab, you can select settings related to the import of images.
In the Language tab, you can select the language.