20  Creating report templates

20.1   General

FLIR Report Studio ships with several different report templates (Microsoft Word *.dotx files). If these templates do not meet your needs, you can create your own custom infrared report templates.

20.1.1  Few or many report templates?

It is not uncommon for a specific template to always be used for a particular customer. If this is the case, you may want to include your customer’s company-specific information in the template, rather than entering it manually after the infrared report has been generated.
However, if infrared reports for several of your customers could be created using one template, or perhaps just a few, company-specific information should probably not be included in the template, since that kind of information can easily be entered when generating the report.

20.1.2  Typical structure

An infrared report template usually consists of the following types of sections:
  • INTRO: The front cover that, for example, can include your company logo and elements of corporate identity, the title of the report, the customer’s name and address, a summary table, and any additional artwork or information that you want to include.
  • DATA: A number of different pages, containing combinations of thermal image objects, digital image objects, field objects, table objects, etc. Multiple DATA sections with different types of content, e.g., “IR only”, Visual only”, ”Two IR”, and “Two IR+Visual”, can be included.
  • FINAL: Your conclusions, recommendations, diagnosis, and summary description.

20.1.3  A note about working in the Microsoft Word‎ environment

Due to the fact that the FLIR Word Add-in is an add-in to Microsoft Word, the existing features you usually use when creating a Microsoft Word document template can be used when creating your report templates.
The FLIR Word Add-in adds a number of commands that are specific to the area of infrared imaging and reporting. These commands are available on the FLIR tab. You use these features, along with the usual Microsoft Word features, when you create infrared report templates.

20.2  Creating a custom infrared report template

You can create a report template in different ways:
  • Customize a basic report template.
  • Modify an existing report template.

20.2.1  Customizing a basic report template

Follow this procedure:

20.2.2  Modifying an existing template—starting from the FLIR Word Add-in‎

Follow this procedure:

20.2.3  Modifying an existing template—starting from the FLIR Report Studio‎ wizard

Follow this procedure:

20.2.4  Adding multiple DATA sections

You can add one or more new DATA sections to the report template, with different types of content, e.g., “IR only”, Visual only”, ”Two IR”, and “Two IR+Visual”.
When using a template with multiple DATA sections in the FLIR Report Studio wizard, a drop-down list is displayed, allowing you to select which section to add images to, see section .

20.2.5  Selecting a template category

You can select one or more categories for the report template.
When saved and imported to the FLIR Report Studio wizard, the report template will appear under the selected category in the left pane of the wizard, see section .

Follow this procedure: