23  Definitions and laws

Term

Definition

Absorption and emission 1
The capacity or ability of an object to absorb incident radiated energy is always the same as the capacity to emit its own energy as radiation
Apparent temperature
uncompensated reading from an infrared instrument, containing all radiation incident on the instrument, regardless of its sources 2
Color palette
assigns different colors to indicate specific levels of apparent temperature. Palettes can provide high or low contrast, depending on the colors used in them
Conduction
direct transfer of thermal energy from molecule to molecule, caused by collisions between the molecules
Convection
heat transfer mode where a fluid is brought into motion, either by gravity or another force, thereby transferring heat from one place to another
Diagnostics
examination of symptoms and syndromes to determine the nature of faults or failures 3
Direction of heat transfer 4
Heat will spontaneously flow from hotter to colder, thereby transferring thermal energy from one place to another 5
Emissivity
ratio of the power radiated by real bodies to the power that is radiated by a blackbody at the same temperature and at the same wavelength 6
Energy conservation 7
The sum of the total energy contents in a closed system is constant
Exitant radiation
radiation that leaves the surface of an object, regardless of its original sources
Heat
thermal energy that is transferred between two objects (systems) due to their difference in temperature
Heat transfer rate 8
The heat transfer rate under steady state conditions is directly proportional to the thermal conductivity of the object, the cross-sectional area of the object through which the heat flows, and the temperature difference between the two ends of the object. It is inversely proportional to the length, or thickness, of the object 9
Incident radiation
radiation that strikes an object from its surroundings
IR thermography
process of acquisition and analysis of thermal information from non-contact thermal imaging devices
Isotherm
replaces certain colors in the scale with a contrasting color. It marks an interval of equal apparent temperature 10
Qualitative thermography
thermography that relies on the analysis of thermal patterns to reveal the existence of and to locate the position of anomalies 11
Quantitative thermography
thermography that uses temperature measurement to determine the seriousness of an anomaly, in order to establish repair priorities 12
Radiative heat transfer
Heat transfer by the emission and absorption of thermal radiation
Reflected apparent temperature
apparent temperature of the environment that is reflected by the target into the IR camera 13
Spatial resolution
ability of an IR camera to resolve small objects or details
Temperature
measure of the average kinetic energy of the molecules and atoms that make up the substance
Thermal energy
total kinetic energy of the molecules that make up the object 14
Thermal gradient
gradual change in temperature over distance 15
Thermal tuning
process of putting the colors of the image on the object of analysis, in order to maximize contrast