13  Managing images and folders

13.1  Grouping files

13.1.1   General

You can group files together, e.g., one infrared image and one digital photo, or one infrared image and a plot. When two files are grouped, a link is created and the images act as a pair through the reporting process.

13.1.2   Procedure

13.2  Saving a sequence file frame as a radiometric *.jpg file

13.2.1   General

You can save a sequence file frame as a radiometric *.jpg image.

13.2.2   Procedure

13.3  Saving a sequence file frame as an *.avi file

13.3.1   General

You can save a sequence file frame as an *.avi file.

13.3.2   Procedure

13.4  Changing the playback speed

13.4.1   General

You can change the playback speed of video clips between –60× and +60×.

13.4.2   Procedure

13.5  Cloning images

13.5.1   General

You can create copies of one or more images. This is called cloning.

13.5.2   Procedure

13.6  Extracting a digital camera photo from a multispectral image

13.6.1   General

For cameras supporting multispectral images, all image modes are included inside a single image file—MSX, thermal, thermal fusion, thermal blending, picture-in-picture, and the digital camera photo.
You can extract a digital camera photo from this multispectral image. The field of view of the extracted photo will match the field of view of the thermal image. Additionally, you can extract a photo at its full field of view.

13.6.2   Procedure : Extracting a photo

13.6.3   Procedure : Extracting a photo at its full field of view

13.7  Enhancing the resolution of an image

13.7.1   General

Some cameras from FLIR Systems support enhancing the resolution of images by using a feature called UltraMax.

13.7.2  Indication of supported images

Supported images are indicated by a special icon on the Library tab. See the bottom right corner in the figure below.
Graphic

13.7.3   Procedure

13.8  Deleting images

13.8.1   General

You can delete one image or a group of images.

13.8.2   Procedure

13.9  Adding a directory

13.9.1   General

You can add a directory to the library.

13.9.2   Procedure

13.10  Deleting a directory

13.10.1   General

You can delete a directory from the library.

13.10.2   Procedure

13.11  Creating a subfolder

13.11.1   General

You can create a subfolder to an existing directory in the library.

13.11.2   Procedure