Automatic
|
Manual
|
Automatic
|
Manual
|
|
Button |
Image mode |
Image example |
|---|---|---|
|
|
Thermal MSX
(Multi Spectral Dynamic Imaging): This mode displays an infrared image where the edges of the objects are enhanced. Note
that the label for each fuse is clearly legible.
|
|
|
|
Thermal
: This mode displays a fully infrared image.
|
|
|
|
Thermal fusion
: This mode displays a digital photo where some parts are displayed in infrared, depending on the temperature limits.
|
|
|
|
Picture-in-picture
: This mode displays an infrared image frame on top of a digital photo.
|
|
|
|
Digital camera
: This mode displays a fully digital photo.
|
|
Follow this procedure:
Add a box or circle measurement tool, see section 14.1 Laying out a measurement tool .
Adjust the size of the box or circle tool to the size of the object, see section 14.3 Resizing a measurement tool .
Right-click the tool and select Local min/max/avg markers. In the dialog box, select the Area check box. This displays the calculated area, based on the distance value, in the Measurements pane.
To change the distance value, click the value field in the Parameters pane, type a new value, and press Enter. The recalculated area, based on the new distance value, is displayed in the Measurements pane.
Follow this procedure:
Add a line measurement tool, see section 14.1 Laying out a measurement tool .
Adjust the size of the line tool to the size of the object, see section 14.3 Resizing a measurement tool .
Right-click the tool and select Local min/max/avg markers. In the dialog box, select the Length check box. This displays the calculated length, based on the distance value, in the Measurements pane.
To change the distance value, click the value field in the Parameters pane, type a new value, and press Enter. The recalculated area, based on the new distance value, is displayed in the Measurements pane.