You can create four types of reports from the program:
An Adobe PDF imagesheet: This is a simple report format that contains only infrared and any associated visual images. The report cannot be edited
further, and radiometric data is not included. For more information, see 17.4 Creating an Adobe PDF imagesheet.
An Adobe PDF report: This is a simple report format that contains infrared images, any associated visual images, and result tables. The report
cannot be edited further, and radiometric data is not included. For more information, see section 17.5 Creating an Adobe PDF report
A non-radiometric Microsoft Word report: This is a more advanced report format that generates the report in the *.docx file format. An active FLIR Tools+ license is required. The report can be extensively edited in Microsoft Word, but radiometric data is not included. For more information, see section 17.6 Creating a non-radiometric Microsoft Word report
A radiometric Microsoft Word report: This is the most advanced report format, and requires an active FLIR Tools+ license. A report in Microsoft Word *.docx file format is generated. Advanced radiometric analysis can be carried out using the FLIR Tools+ features in Microsoft Word. For more information, see section 17.7 Creating a radiometric Microsoft Word report
Prior to working with reports, you need to set a default report template. A maximum of two default report templates can be
set. These templates will then be used when clicking Generate report on the Library tab.
Follow this procedure:
NoteThe first two rows of templates apply to FLIR Tools+ only.
On the Library tab, click
. This will display the available report templates.
Right-click a report template and click Set as default report template.
17.3 Saving a report in the intermediary *.repx format
Follow this procedure:
On the Library tab, select the image or images that you want to include in your report.
Right-click the image or images and select Create report.
Under Page setup in the right pane, select the page size and logo that you want to use.
On the report, double-click the header and/or footer to add any header/footer text that you want to use.
Click Save or Save As to save the report in FLIR Systems*.repx file format.
17.4 Creating an Adobe PDF imagesheet
Follow this procedure:
On the Library tab, select the image or images that you want to include in your imagesheet.
Right-click the image or images and select Create imagesheet.
Under Page setup on the right pane, select the page size and logo that you want to use.
Under Layout on the right pane, click the page layout that you want to use.
On the imagesheet, double-click the header and/or footer to add any header/footer text that you want to use.
Click Export to export the imagesheet as a PDF file.
17.5 Creating an Adobe PDF report
NoteThis procedure assumes that an Adobe PDF report has been set as a default template.
Follow this procedure:
On the Library tab, select the image or images that you want to include in your report.
Right-click the image or images and select Create report. This displays the Report tab.
At this stage, you have the option to do one or more of the following:
Drag a group of images, photos, or text annotations into a report.
Drag single images, photos, or tables into a report.
Reorder the pages in the report.
Enter text in a report using textboxes.
Create and edit text annotations.
Edit image descriptions.
Add and edit a header or footer in a report.
Move and delete images, photos, text annotations, and tables in a report.
Resize images in a report.
Update measurements in an infrared image and see updates instantly in the result table.
Zoom into and out of a report page.
Add arrow markers to the image or any other object in the report.
Edit an image from the report by double-clicking the image.
In the Save PDF as dialog box, select a location and type a filename.
Click OK.
17.6 Creating a non-radiometric Microsoft Word report
Note
This procedure assumes that a non-radiometric Microsoft Word report has been set as a default template.
This procedure requires an active FLIR Tools+ license.
Follow this procedure:
On the Library tab, select the image or images that you want to include in your report.
Right-click the image or images and select Create report.
In the dialog box that appears, enter the customer information and information about the inspection in the right column. Use
the TAB key to go between fields.
Click OK. The information you entered in this dialog box will now populate the corresponding placeholders in the report.
Once the report is generated, the report can be further edited in Microsoft Word.
17.6.1 Creating “Rapid Report” shortcuts
17.6.1.1 General
For non-radiometric Microsoft Word reports, you can create Desktop shortcuts called “Rapid Report” shortcuts. You can then drag-and-drop images to this shortcut
to create reports without starting FLIR Tools+.
17.6.1.2 Procedure
Follow this procedure:
On the Library tab, click
. This will display the available report templates.
Right-click one of the Word templates (Express export) and select Create Rapid Report shortcut.
17.7 Creating a radiometric Microsoft Word report
Note
This procedure assumes that a radiometric Microsoft Word report has been set as a default template.
This procedure requires an active FLIR Tools+ license.
Follow this procedure:
On the Library tab, select the image or images that you want to include in your report.
Right-click the image or images and select Create report.
In the dialog box that appears, enter the customer information and information about the inspection in the right column. Use
the TAB key to go between fields.
Click OK. The information you entered in this dialog box will now populate the corresponding placeholders in the report.
Once the report is generated, advanced analysis can be carried out using the FLIR Tools+ features in Microsoft Word.
NoteThis workflow assumes that the report properties are prefixed with an underscore (_), as they are for the standard report
templates.
However, if you have created your own custom templates, you may have created report properties with a different prefix, e.g.,
using a percentage sign (%), a dollar sign ($), a hash sign (#), or the whole or part of your company name (e.g., “ACME”).
To have these properties show up when you generate the report, you need to update the property FLIR_ReportPropertyPrefix in Microsoft Word. For more information about this, see section 18.3.4 Changing the prefix for a report property