Follow this procedure:
Push the joystick to display the menu system.
Use the joystick to go to
(Settings).
Push the joystick to display the Settings menu.
Select Device settings and push the joystick.
Select Compass and push the joystick.
Select Compass. If the Compass check box is unchecked, push the joystick to enable the compass.
Select Calibrate compass and push the joystick. Follow the on-screen instructions.

Follow this procedure:
Push the joystick to display the menu system.
Use the joystick to go to
(Settings).
Push the joystick to display the Settings menu.
Select Device settings and push the joystick.
Select Set up camera and push the joystick.
Select Lamp & laser and push the joystick.
Select Enable lamp & laser. If the check box is unchecked, push the joystick to enable the camera lamp.
Select Use lamp as flash. If the check box is unchecked, push the joystick to activate the flash function.