10  Navigating the menu system

10.1  Figure

Graphic
Graphic

10.2  Explanation

The figure above shows the two ways to navigate the menu system in the camera:
  • Using the index finger or a stylus pen specially designed for capacitive touch usage to navigate the menu system (left)‎.
  • Using the joystick to navigate the menu system (right)‎.
You can also use a combination of the two.
In this manual it is assumed that the joystick is used,‎ but most tasks can also be carried out using the index finger or a stylus pen.