11  Pairing Bluetooth‎ devices

11.1  General

Before you can use a Bluetooth device with the camera,‎ you need to pair the devices.

11.2  Procedure

    Follow this procedure:
  1. Push the joystick to display the menu system.
  2. Use the joystick to go to icon (Settings)‎.
  3. Push the joystick to display the Settings menu.
  4. Select Device settings and push the joystick.
  5. Select Bluetooth including METERLiNK and push the joystick.
  6. If the Bluetooth check box is unchecked,‎ push the joystick to activate Bluetooth.
  7. Select Scan for Bluetooth devices and push the joystick.
  8. Wait until a list of available devices is displayed. This will take about 15 seconds.
  9. When a Bluetooth device is found,‎ select the device to add it,‎ and begin the pairing procedure. The device is then ready to be used.