15  Working with image modes

15.1  General

The camera captures both thermal and visual images at the same time. By your choice of image mode,‎ you select which type of image to display on the screen.
The camera supports the following image modes:
  • Thermal MSX (Multi Spectral Dynamic Imaging)‎: The camera displays infrared images where the edges of the objects are enhanced with visual image details.
  • Thermal: A full infrared image is displayed.
  • Picture in picture: An infrared image frame is displayed on top of the visual image.
  • Digital camera: The visual image captured by the digital camera is displayed.

15.2  Image examples

This table explains the different types of image modes.

Image mode

Image

Thermal
Graphic
Thermal MSX
Graphic
Picture in picture
Graphic
Digital camera
Graphic

15.3  Selecting the image mode

Follow this procedure:

Push the joystick to display the menu system.

Use the joystick to go to icon (Image mode)‎.

Push the joystick to display a submenu.

Use the joystick to go to one of the image modes:

  • icon (Thermal MSX)‎
  • icon (Thermal)‎
  • icon (Picture in picture)‎
  • icon (Digital camera)‎

Push the joystick confirm.

If Picture in picture mode is selected,‎ you can at this point move and resize the image frame using the touch screen.