|
Color alarm |
Image |
|---|---|
|
Above alarm
|
![]() |
|
Below alarm
|
![]() |
|
Interval alarm
|
![]() |
|
Condensation alarm
|
![]() |
|
Insulation alarm
|
![]() |
Follow this procedure:
Push the joystick to display the menu system.
Use the joystick to go to
(Color).
Push the joystick to display a submenu. Use the joystick to select the type of alarm:
Push the joystick. The threshold temperature is displayed at the bottom of the screen.
To change the threshold temperature, do the following:
Follow this procedure:
Push the joystick to display the menu system.
Use the joystick to go to
(Color).
Push the joystick to display a submenu. Use the joystick to select the type of alarm:
Push the joystick. This displays a dialog box where you can define the settings for the alarm.
For the Condensation alarm, the following parameters can be set:
For the Insulation alarm, the following parameters can be set:
Push the joystick. This closes the dialog box.