21  Recording video clips

21.1  General

You can record and save video clips to the memory card.

21.2  Procedure

Follow this procedure:

Push the joystick to display the menu system.

Use the joystick to go to icon (Recording mode)‎.

Push the joystick. This displays a submenu.

Select icon (Video)‎ and push the joystick.

Do the following:

  • To start a recording,‎ push and release the Autofocus/Save button. A counter at the top of the screen displays the duration of the recording.
  • To stop a recording,‎ push and release the Autofocus/Save button.

The recording is automatically saved to the image archive,‎ where you can play or delete it.