23  Changing settings

23.1  General

The Settings menu includes the following:
  • Define user presets
  • Save options
  • Programmable button
  • Reset options
  • Device settings

23.1.1  Define user presets

  • Define preset 1
  • Define preset 2

23.1.2  Save options

  • Preview image before saving
  • Add annotation after saving
  • Image resolution
  • Video compression
  • Photo as separate JPEG

23.1.3  Programmable button

  • No action
  • Hide graphics
  • Calibrate
  • Switch Thermal <> Digital camera
  • Switch Thermal <> Thermal MSX
  • Switch 1x zoom <> Max zoom
  • Switch between two latest palettes
  • Switch temperature range

23.1.4  Reset options

  • Reset default camera mode...
  • Reset device settings to factory default...
  • Delete all saved images...

23.1.5  Device settings

  • Set up camera
    • Camera temperature range: The temperature range used for measuring objects. You must change the temperature range according to the expected temperature of the object you are inspecting.
    • Auto orientation
    • Display intensity
    • Lamp & laser
    • Auto power off
    • Emissivity mode
    • Video output format
    • Calibrate touchscreen
    • Screening mode
  • Wi-Fi: For more information,‎ see 12 Configuring Wi-Fi.
  • Compass
  • Bluetooth including METERLiNK: For more information,‎ see 11 Pairing Bluetooth‎ devices.
  • Language,‎ time & units
  • Camera information: Information about the model,‎ serial number,‎ part number,‎ and software versions. No changes can be made.

23.2  Procedure

Follow this procedure:

Push the joystick to display the menu system.

Use the joystick to go to icon (Settings)‎.

Push the joystick to display the Settings menu.

Use the joystick to select the setting you want to change.

To exit the Settings menu or a submenu,‎ push the Back button icon.