12  Configuring Wi-Fi

12.1  General

Depending on your camera configuration,‎ you can connect the camera to a wireless local area network (WLAN)‎ using Wi-Fi,‎ or let the camera provide Wi-Fi access to another device.
You can connect the camera in two different ways:
  • Most common use: Setting up a peer-to-peer connection (also called an ad hoc or P2P connection)‎. This method is primarily used with other devices,‎ e.g.,‎ an iPhone or iPad.
  • Less common use: Connecting the camera to a WLAN.

12.2  Setting up a peer-to-peer connection (most common use)‎

    Follow this procedure:
  1. Push the joystick to display the menu system.
  2. Use the joystick to go to icon (Settings)‎.
  3. Push the joystick to display the Settings menu.
  4. Select Device settings and push the joystick.
  5. Select Wi-Fi and push the joystick.
  6. Select Share and push the joystick.
  7. (Optional step.)‎ To display and change the parameters,‎ select Settings and push the joystick.
    • To change the channel (the channel that the camera is broadcasting on)‎,‎ select Channel and push the joystick.
    • To activate WEP (encryption algorithm)‎,‎ select WEP and push the joystick. This will check the WEP check box.
    • To change the WEP password,‎ select Password and push the joystick.

12.3  Connecting the camera to a wireless local area network (less common use)‎

    Follow this procedure:
  1. Push the joystick to display the menu system.
  2. Use the joystick to go to icon (Settings)‎.
  3. Push the joystick to display the Settings menu.
  4. Select Device settings and push the joystick.
  5. Select Wi-Fi and push the joystick.
  6. Select Connect to network and push the joystick.
  7. To display a list of the available networks,‎ select Networks and push the joystick.
  8. Select one of the available networks.
    Password-protected networks are indicated with a padlock icon,‎ and for these you will need to enter a password.