| WARNING | |
|
Applicability: Class B digital devices.
This equipment has been tested and found to comply with the limits for a Class B digital device, pursuant to Part 15 of the
FCC Rules. These limits are designed to provide reasonable protection against harmful interference in a residential installation.
This equipment generates, uses and can radiate radio frequency energy and, if not installed and used in accordance with
the instructions, may cause harmful interference to radio communications. However, there is no guarantee that interference
will not occur in a particular installation. If this equipment does cause harmful interference to radio or television reception,
which can be determined by turning the equipment off and on, the user is encouraged to try to correct the interference by
one or more of the following measures:
|
|
| WARNING | |
|
Applicability: Digital devices subject to 15.19/RSS-210.
NOTICE: This device complies with Part 15 of the FCC Rules and with RSS-210 of Industry Canada. Operation is subject to the following
two conditions:
|
|
| WARNING | |
|
Applicability: Digital devices subject to 15.21.
NOTICE: Changes or modifications made to this equipment not expressly approved by FLIR Systems may void the FCC authorization to operate this equipment.
|
|
| WARNING | |
|
Applicability: Digital devices subject to 2.1091/2.1093/OET Bulletin 65.
Radiofrequency radiation exposure Information: The radiated output power of the device is below the FCC/IC radio frequency exposure limits. Nevertheless, the device shall
be used in such a manner that the potential for human contact during normal operation is minimized.
|
|
| WARNING | |
|
Applicability: Cameras with one or more laser pointers.
Do not look directly into the laser beam. The laser beam can cause eye irritation.
|
|
| WARNING | |
|
Applicability: Cameras with one or more batteries.
Do not disassemble or do a modification to the battery. The battery contains safety and protection devices which, if damage
occurs, can cause the battery to become hot, or cause an explosion or an ignition.
|
|
| WARNING | |
|
Applicability: Cameras with one or more batteries.
If there is a leak from the battery and you get the fluid in your eyes, do not rub your eyes. Flush well with water and immediately
get medical care. The battery fluid can cause injury to your eyes if you do not do this.
|
|
| WARNING | |
|
Applicability: Cameras with one or more batteries.
Do not continue to charge the battery if it does not become charged in the specified charging time. If you continue to charge
the battery, it can become hot and cause an explosion or ignition. Injury to persons can occur.
|
|
| WARNING | |
|
Applicability: Cameras with one or more batteries.
Only use the correct equipment to remove the electrical power from the battery. If you do not use the correct equipment,
you can decrease the performance or the life cycle of the battery. If you do not use the correct equipment, an incorrect
flow of current to the battery can occur. This can cause the battery to become hot, or cause an explosion. Injury to persons
can occur.
|
|
| WARNING | |
|
Make sure that you read all applicable MSDS (Material Safety Data Sheets) and warning labels on containers before you use
a liquid. The liquids can be dangerous. Injury to persons can occur.
|
|
| CAUTION | |
|
Do not point the infrared camera (with or without the lens cover) at strong energy sources, for example, devices that cause
laser radiation, or the sun. This can have an unwanted effect on the accuracy of the camera. It can also cause damage to
the detector in the camera.
|
|
| CAUTION | |
|
Do not use the camera in temperatures more than +50°C (+122°F), unless other information is specified in the user documentation
or technical data. High temperatures can cause damage to the camera.
|
|
| CAUTION | |
|
Applicability: Cameras with one or more laser pointers.
To prevent damage, put the protective cap on the laser pointer when you do not operate the laser pointer. Damage to the laser
pointer can occur if you do not do this.
|
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
Do not attach the batteries directly to a car’s cigarette lighter socket, unless FLIR Systems supplies a specific adapter to connect the batteries to a cigarette lighter socket. Damage to the batteries can occur.
|
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
Do not connect the positive terminal and the negative terminal of the battery to each other with a metal object (such as wire).
Damage to the batteries can occur.
|
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
Do not get water or salt water on the battery, or permit the battery to become wet. Damage to the batteries can occur. |
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
Do not make holes in the battery with objects. Damage to the battery can occur. |
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
Do not hit the battery with a hammer. Damage to the battery can occur. |
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
Do not put your foot on the battery, hit it or cause shocks to it. Damage to the battery can occur. |
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
Do not put the batteries in or near a fire, or into direct sunlight. When the battery becomes hot, the built-in safety equipment
becomes energized and can stop the battery charging procedure. If the battery becomes hot, damage can occur to the safety
equipment and this can cause more heat, damage or ignition of the battery.
|
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
Do not put the battery on a fire or increase the temperature of the battery with heat. Damage to the battery and injury to
persons can occur.
|
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
Do not put the battery on or near fires, stoves, or other high-temperature locations. Damage to the battery and injury to
persons can occur.
|
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
Do not solder directly onto the battery. Damage to the battery can occur. |
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
Do not use the battery if, when you use, charge, or put the battery in storage, there is an unusual smell from the battery,
the battery feels hot, changes color, changes shape, or is in an unusual condition. Speak with your sales office if one
or more of these problems occurs. Damage to the battery and injury to persons can occur.
|
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
Only use a specified battery charger when you charge the battery. Damage to the battery can occur if you do not do this. |
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
Only use a specified battery for the camera. Damage to the camera and the battery can occur if you do not do this. |
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
The temperature range through which you can charge the battery is ±0°C to +45°C (+32°F to +113°F), unless other information is specified in the user documentation or technical data. If you charge the battery at temperatures
out of this range, it can cause the battery to become hot or to break. It can also decrease the performance or the life cycle
of the battery.
|
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
The temperature range through which you can remove the electrical power from the battery is -15°C to +50°C (+5°F to +122°F), unless other information is specified in the user documentation or technical data. If you operate the battery out of this
temperature range, it can decrease the performance or the life cycle of the battery.
|
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
When the battery is worn, apply insulation to the terminals with adhesive tape or equivalent materials before you discard
it. Damage to the battery and injury to persons can occur if you do not do this.
|
|
| CAUTION | |
|
Applicability: Cameras with one or more batteries.
Remove any water or moisture on the battery before you install it. Damage to the battery can occur if you do not do this. |
|
| CAUTION | |
|
Do not apply solvents or equivalent liquids to the camera, the cables, or other items. Damage to the battery and injury
to persons can occur.
|
|
| CAUTION | |
|
Be careful when you clean the infrared lens. The lens has an anti-reflective coating which is easily damaged. Damage to the
infrared lens can occur.
|
|
| CAUTION | |
|
Do not use too much force to clean the infrared lens. This can cause damage to the anti-reflective coating. |
|
| Note | |
|
The encapsulation rating is only applicable when all the openings on the camera are sealed with their correct covers, hatches,
or caps. This includes the compartments for data storage, batteries, and connectors.
|
|