Follow this procedure:
Enable the screening mode by selecting
(Settings) > Device settings > Set up camera > Screening mode = On.
Push the joystick to display the menu system.
Use the joystick to go to
(Recording mode).
Push the joystick. This displays a submenu.
Select
(Screening).
Push the joystick. This displays a dialog box where you can define the settings for the alarm.
Push the joystick. This closes the dialog box.
Aim the camera toward a point of interest. The object should be within the frame of the measurement box.
Push and hold the programmable button
to reset the sampled average.
Push the programmable button
to sample.
Aim the camera toward more points of interest. Sample 10 times to build up a sample base by pushing the programmable button
.
The alarm is now set up and ready to use. Occasionally record a few samples if the alarm is used for a long time or if the conditions change.