FLIR T4xx series
1 Disclaimers
2 Safety information
3 Notice to user
4 Customer help
5 Quick start guide
6 List of accessories and services
7 A note about ergonomics
8 Camera parts
9 Screen elements
10 Navigating the menu system
11 Pairing Bluetooth devices
12 Configuring Wi-Fi
13 Handling the camera
13.1 Charging the battery
13.1.1 General
13.1.2 Using the combined power supply and battery charger to charge the battery when it is inside the camera
13.1.3 Using the combined power supply and battery charger to charge the battery when it is outside the camera
13.1.4 Using the stand-alone battery charger to charge the battery
13.2 Inserting the battery
13.3 Removing the battery
13.4 Turning on and turning off the camera
13.5 Adjusting the angle of lens
13.6 Adjusting the infrared camera focus
13.7 Mounting an additional lens
13.8 Removing an additional infrared lens
13.9 Attaching the sunshield
13.10 Using the laser pointer
13.11 Calibrating the compass
13.12 Calibrating the touchscreen LCD
13.13 Using the camera lamp as a flash
14 Working with images
14.1 Saving an image
14.2 Previewing an image
14.3 Opening a saved image
14.4 Editing a saved image
14.5 Adjusting an infrared image
14.6 Performing a non-uniformity correction (NUC)
14.7 Changing the temperature range
14.8 Hiding overlay graphics (programmable button)
14.9 Changing the color palette
14.10 Deleting an image
14.11 Deleting all images
14.12 Creating a PDF report in the camera
15 Working with image modes
16 Working with measurement tools
16.1 General
16.2 Adding/removing measurement tools
16.3 Working with user presets
16.4 Resizing or moving a measurement tool
16.5 Changing object parameters
16.6 Displaying values in the result table and displaying a graph
16.7 Creating and setting up a difference calculation
16.8 Setting a measurement alarm
17 Fetching data from external FLIR meters
18 Working with color alarms and isotherms
19 Annotating images
20 Programming the camera (time lapse)
21 Recording video clips
22 Screening alarm
23 Changing settings
24 Technical data
24.1 Online field-of-view calculator
24.2 Note about technical data
24.3 Note about authoritative versions
24.4 FLIR T420 (incl. Wi-Fi and 15° lens)
24.5 FLIR T420 (incl. Wi-Fi and 45° lens)
24.6 FLIR T420 (incl. Wi-Fi and Ext. cal.) (60 Hz)
24.7 FLIR T420 (incl. Wi-Fi)
24.8 FLIR T420 with SC kit (incl. Wi-Fi, incl. 45° lens)
24.9 FLIR T420bx (incl. Wi-Fi and Ext. cal.) (60 Hz)
24.10 FLIR T420bx (incl. Wi-Fi)
24.11 FLIR T420bx 25° and 15° w/case
24.12 FLIR T420bx 25° and 45° w/case
24.13 FLIR T430sc (incl. Wi-Fi)
24.14 FLIR T430sc with SC kit (incl. Wi-Fi)
24.15 FLIR T440 (incl. Wi-Fi and Ext. cal.) (60 Hz)
24.16 FLIR T440 (incl. Wi-Fi and 15° lens)
24.17 FLIR T440 (incl. Wi-Fi and 45° lens)
24.18 FLIR T440 (incl. Wi-Fi)
24.19 FLIR T440bx (incl. Wi-Fi and Ext. cal.) (60 Hz)
24.20 FLIR T440bx (incl. Wi-Fi)
24.21 FLIR T440bx 25° and 15° w/case
24.22 FLIR T440bx 25° and 45° w/case
24.23 FLIR T450sc (incl. Wi-Fi)
24.24 FLIR T450sc 25° and 45° w/case
24.25 FLIR T460 (incl. Wi-Fi and Ext. cal.)
24.26 FLIR T460 (incl. Wi-Fi)
24.27 FLIR T460 25° and 15° w/case
24.28 FLIR T460 25° and 45° w/case
25 Pin configurations
26 Mechanical drawings
27 CE Declaration of conformity
28 Cleaning the camera
29 Application examples
30 About FLIR Systems
31 Glossary
32 Thermographic measurement techniques
33 History of infrared technology
34 Theory of thermography
35 The measurement formula
36 Emissivity tables
Admin