| DANGER | |
|
Applicability: FLIR A3xx pt & G300 pt.
Do not install the unit in lightning weather. A lightning strike can hit the unit and cause injury or death.
|
|
| DANGER | |
|
Applicability: FLIR A3xx pt & G300 pt.
Be careful when you install or do an inspection of the unit at high heights. The unit can move suddenly and this can cause
you to fall. This can cause injury or death.
|
|
| DANGER | |
|
Applicability: FLIR A3xx pt & G300 pt.
Make sure that you use the industry standard safety procedures when you install or do an inspection of the unit at high heights.
If you do not use the industry standard safety procedures, this can cause you to fall. This can cause injury or death.
|
|
| WARNING | |
|
Make sure that you read all applicable MSDS (Material Safety Data Sheets) and warning labels on containers before you use
a liquid. The liquids can be dangerous. Injury to persons can occur.
|
|
| WARNING | |
|
Applicability: FLIR A3xx pt & G300 pt.
Be careful when you lift the unit when it is not energized. This can cause the parts of the unit to move freely and cause
injury.
|
|
| WARNING | |
|
Applicability: FLIR A3xx pt & G300 pt.
Do not go near the unit when it is energized. The unit can move suddenly and cause injury.
|
|
| WARNING | |
|
Applicability: FLIR A3xx pt & G300 pt.
Do not go near the unit during the startup. The unit can move suddenly and cause injury.
|
|
| WARNING | |
|
Applicability: FLIR A3xx pt & G300 pt.
A minimum of two persons are necessary to lift the unit. The unit can cause injury when the center of gravity moves.
|
|
| WARNING | |
|
Applicability: FLIR A3xx pt & G300 pt.
Make sure that you install the unit safely. If you do not install it safely, the unit can fall down and cause injury.
|
|
| WARNING | |
|
Applicability: FLIR A3xx pt & G300 pt.
If the IR or the TV window breaks, do not touch the broken pieces. The pieces can cause injury.
|
|
| WARNING | |
|
Applicability: FLIR A3xx pt & G300 pt.
Be careful when you touch the unit. Some parts can be sharp and cause injury.
|
|
| CAUTION | |
|
Do not point the infrared camera (with or without the lens cover) at strong energy sources, for example, devices that cause
laser radiation, or the sun. This can have an unwanted effect on the accuracy of the camera. It can also cause damage to
the detector in the camera.
|
|
| CAUTION | |
|
Do not use the camera in temperatures more than +50°C (+122°F), unless other information is specified in the user documentation
or technical data. High temperatures can cause damage to the camera.
|
|
| CAUTION | |
|
Do not apply solvents or equivalent liquids to the camera, the cables, or other items. Damage to the battery and injury
to persons can occur.
|
|
| CAUTION | |
|
Be careful when you clean the infrared lens. The lens has an anti-reflective coating which is easily damaged. Damage to the
infrared lens can occur.
|
|
| CAUTION | |
|
Do not use too much force to clean the infrared lens. This can cause damage to the anti-reflective coating. |
|
| CAUTION | |
|
Applicability: Cameras with an automatic shutter that can be disabled.
Do not disable the automatic shutter in the camera for a long time period (a maximum of 30 minutes is typical). If you disable
the shutter for a longer time period, damage to the detector can occur.
|
|
| Note | |
|
The encapsulation rating is only applicable when all the openings on the camera are sealed with their correct covers, hatches,
or caps. This includes the compartments for data storage, batteries, and connectors.
|
|
| CAUTION | |
|
Applicability: Cameras where you can remove the lens and expose the infrared detector.
Do not use the pressurized air from the pneumatic air systems in a workshop when you remove dust from the detector. The air
contains oil mist to lubricate the pneumatic tools and the pressure is too high. Damage to the detector can occur.
|
|