Prior to installing the camera, use a bench test to verify camera operation and to configure the camera for the local network.
The camera can be controlled through either serial or IP communications.
9.2 IP communications
As shipped from the factory, the FLIR A3xx pt series camera has an IP address of 192.168.250.116 with a netmask of 255.255.255.0.
Follow this procedure:
- Configure a laptop or PC with another IP address from this network (i.e., 192.168.250.xxx).
- Connect the camera and the laptop to the same Ethernet switch (or back-to-back with an Ethernet crossover cable). In some
cases, a straight Ethernet cable can be used because many PCs have auto detect Ethernet interfaces.
- Open a web browser, enter 192.168.250.116 in the address bar, and press Enter. If the following screen appears, then you have established IP communications with
the camera.
Note The credentials are the following:
- User name: admin
- Password: fliradmin