13  About FLIR Systems

FLIR Systems was established in 1978 to pioneer the development of high-‎performance infrared imaging systems,‎ and is the world leader in the design,‎ manufacture,‎ and marketing of thermal imaging systems for a wide variety of commercial,‎ industrial,‎ and government applications. Today,‎ FLIR Systems embraces five major companies with outstanding achievements in infrared technology since 1958—the Swedish AGEMA Infrared Systems (formerly AGA Infrared Systems)‎,‎ the three United States companies Indigo Systems,‎ FSI,‎ and Inframetrics,‎ and the French company Cedip.
Since 2007,‎ FLIR Systems has acquired several companies with world-‎leading expertise in sensor technologies:
Graphic

Figure 13.1  Patent documents from the early 1960s

FLIR Systems has three manufacturing plants in the United States (Portland,‎ OR,‎ Boston,‎ MA,‎ Santa Barbara,‎ CA)‎ and one in Sweden (Stockholm)‎. Since 2007 there is also a manufacturing plant in Tallinn,‎ Estonia. Direct sales offices in Belgium,‎ Brazil,‎ China,‎ France,‎ Germany,‎ Great Britain,‎ Hong Kong,‎ Italy,‎ Japan,‎ Korea,‎ Sweden,‎ and the USA—together with a worldwide network of agents and distributors—support our international customer base.
FLIR Systems is at the forefront of innovation in the infrared camera industry. We anticipate market demand by constantly improving our existing cameras and developing new ones. The company has set milestones in product design and development such as the introduction of the first battery-‎operated portable camera for industrial inspections,‎ and the first uncooled infrared camera,‎ to mention just two innovations.
Graphic

Figure 13.2  1969: Thermovision Model 661. The camera weighed approximately 25 kg (55 lb.)‎,‎ the oscilloscope 20 kg (44 lb.)‎,‎ and the tripod 15 kg (33 lb.)‎. The operator also needed a 220 VAC generator set,‎ and a 10 L (2.6 US gallon)‎ jar with liquid nitrogen. To the left of the oscilloscope the Polaroid attachment (6 kg/13 lb.)‎ can be seen.

Graphic

Figure 13.3  2015: FLIR One,‎ an accessory to iPhone and Android mobile phones. Weight: 90 g (3.2 oz.)‎.

FLIR Systems manufactures all vital mechanical and electronic components of the camera systems itself. From detector design and manufacturing,‎ to lenses and system electronics,‎ to final testing and calibration,‎ all production steps are carried out and supervised by our own engineers. The in-‎depth expertise of these infrared specialists ensures the accuracy and reliability of all vital components that are assembled into your infrared camera.

13.1  More than just an infrared camera

At FLIR Systems we recognize that our job is to go beyond just producing the best infrared camera systems. We are committed to enabling all users of our infrared camera systems to work more productively by providing them with the most powerful camera–software combination. Especially tailored software for predictive maintenance,‎ R & D,‎ and process monitoring is developed in-‎house. Most software is available in a wide variety of languages.
We support all our infrared cameras with a wide variety of accessories to adapt your equipment to the most demanding infrared applications.

13.2  Sharing our knowledge

Although our cameras are designed to be very user-‎friendly,‎ there is a lot more to thermography than just knowing how to handle a camera. Therefore,‎ FLIR Systems has founded the Infrared Training Center (ITC)‎,‎ a separate business unit,‎ that provides certified training courses. Attending one of the ITC courses will give you a truly hands-‎on learning experience.
The staff of the ITC are also there to provide you with any application support you may need in putting infrared theory into practice.

13.3  Supporting our customers

FLIR Systems operates a worldwide service network to keep your camera running at all times. If you discover a problem with your camera,‎ local service centers have all the equipment and expertise to solve it within the shortest possible time. Therefore,‎ there is no need to send your camera to the other side of the world or to talk to someone who does not speak your language.