12.5.1 General
Draft can be found under baseboards, around door and window casings, and above ceiling trim. This type of draft is often
possible to see with an infrared camera, as a cooler airstream cools down the surrounding surface.
When you are investigating draft in a house, there should be sub-atmospheric pressure in the house. Close all doors, windows,
and ventilation ducts, and allow the kitchen fan to run for a while before you take the infrared images.
An infrared image of draft often shows a typical stream pattern. You can see this stream pattern clearly in the picture below.
Also keep in mind that drafts can be concealed by heat from floor heating circuits.