7  Description

7.1  View from the front

7.1.1  Figure

Graphic

7.1.2  Explanation

  1. Infrared lens.
  2. Trigger.

7.2  View from the rear

7.2.1  Figure

Graphic

7.2.2  Explanation

  1. Camera screen.
  2. Five-way button.
    Function:
    • Push the MID button to turn on the camera.
    • Push and hold the MID button for more than 2 seconds to turn off the camera.
    • Push the MID button to display the menu system.
    • Use the UP/DOWN and LEFT/RIGHT buttons to navigate in the menu system.
    • Push the MID button to confirm actions in the menu system.
  3. Battery compartment.
  4. Lanyard access.

7.3  Screen elements

7.3.1  Figure

Graphic

7.3.2  Explanation

  1. Crosshair temperature.
  2. Battery status icon (visible when the menu is displayed)‎.
  3. Crosshair.
  4. Main menu.

7.3.3  Status icons and indicators

icon
The battery low icon indicates that the batteries must be replaced.