8  Operation

8.1  Replacing the batteries

If the battery low icon icon is displayed or if the camera does not power on,‎ you must replace the batteries.

Follow this procedure:

Turn off the camera.

Lift up the battery compartment cover.

Graphic

Remove the battery pack.

Replace the three standard AAA batteries,‎ ensuring correct polarity.

Put the battery pack into the battery compartment.

Push down and secure the battery compartment cover. The cover makes a click when it locks in place.

8.2  Turning on and turning off the camera

  • To turn on the camera,‎ push the MID button.
  • To turn off the camera,‎ push and hold the MID button for more than 2 seconds.

8.3  Selecting the camera mode

8.3.1  General

The camera supports the following modes:
  • Iron: The camera uses a color palette to display different temperatures in the image. A crosshair indicates the center of the image. The temperature at the position of the crosshair is displayed.
  • Hot: A contrasting color is applied to the hottest parts of the image. A red crosshair indicates the spot with the highest temperature. The temperature at the position of the hot spot is displayed.
  • Cold: A contrasting color is applied to the coldest parts of the image. A blue crosshair indicates the spot with the lowest temperature. The temperature at the position of the cold spot is displayed.

Camera mode

Image

Iron
Graphic
Hot
Graphic
Cold
Graphic

8.3.2  Procedure

Follow this procedure:

Push the MID button to display the menu system.

Use the LEFT/RIGHT buttons to go to the icon icon.

Push the MID button. This displays a submenu.

Use the LEFT/RIGHT buttons to select the camera mode:

  • icon Iron
  • icon Hot
  • icon Cold

Push the MID button to confirm and return to the live image.

8.4  Saving an image

8.4.1  General

You can save up to 25 images to the internal memory. The images are saved in a first-in-first-out manner. This means that if the memory is full,‎ the oldest image will be deleted when a new image is saved.
The images are saved with the current camera mode and with the temperature reading displayed.
Graphic

8.4.2  Procedure

Follow this procedure:

Aim the camera toward a point of interest.

Pull the trigger to freeze and save the image. When saving is completed,‎ after about 2 seconds,‎ the live image is displayed.

8.5  Viewing a saved image

8.5.1  General

When you save an image,‎ the image file is stored in the internal memory. To display the image again,‎ open it from the image archive.

8.5.2  Procedure

Follow this procedure:

Push the MID button to display the menu system.

Use the LEFT/RIGHT buttons to go to the icon icon.

Push the MID button to open the image archive.

Use the LEFT/RIGHT buttons to scroll through the saved images.

To close the image archive,‎ do one of the following:

  • Pull the trigger.
  • Push the MID button to display a submenu. Select the icon icon and push the MID button.

8.6  Deleting an image

8.6.1  General

You can delete an image from the internal memory.

8.6.2  Procedure

Follow this procedure:

Push the MID button to display the menu system.

Use the LEFT/RIGHT buttons to go to the icon icon.

Push the MID button to open the image archive.

Use the LEFT/RIGHT buttons to select the image you want to delete.

Push the MID button to display a submenu.

Select the icon icon and push the MID button. This displays a dialog box.

Select the icon icon and push the MID button.

Push the MID button to delete the image.

8.7  Deleting all images

You can delete all image files from the internal memory. For more information,‎ see section 8.8 Changing the settings.

8.8  Changing the settings

8.8.1  General

You can change the settings in the camera. You do this on the Settings menu.
Graphic

8.8.2  Emissivity

Emissivity is a measure of the amount of radiation coming from an object,‎ compared with that from a perfect blackbody of the same temperature.
Emissivity values normally range from 0.1 to 0.95. A highly polished (mirror)‎ surface falls below 0.1,‎ while an oxidized or painted surface has a higher emissivity. Oil-based paint,‎ regardless of its color in the visible spectrum,‎ has an emissivity of over 0.9 in the infrared. Human skin has an emissivity 0.97–0.98. Non-oxidized metals represent an extreme case of perfect opacity and high reflexivity,‎ which does not vary greatly with wavelength. Consequently,‎ the emissivity of metals is low—only increasing with temperature. For non-metals,‎ emissivity tends to be high,‎ and decreases with temperature.
For accurate measurements,‎ you must select the correct emissivity setting. You can select a value between 0.01 and 0.99. For a list of emissivity data for different materials,‎ see section 16 Emissivity tables.

8.8.3  Temperature unit

Available options for the Temp unit setting:
  • °C (Celsius)‎
  • °F (Fahrenheit)‎

8.8.4  Auto off

The Auto off function automatically turns off the camera after a selectable period of inactivity.
Available options:
  • 5 min (5 minutes)‎
  • 10 min (10 minutes)‎
  • (the camera will not turn off automatically)‎

8.8.5  Delete all

The Delete all action deletes all images from the internal memory.

8.8.6  Restore

The Restore action restores all the settings to the factory default.

8.8.7  Procedure

Follow this procedure:

Push the MID button to display the menu system.

Use the LEFT/RIGHT buttons to go to the icon icon.

Push the MID button. This displays the Settings menu.

Use the UP/DOWN buttons to go to the desired setting/action.

Push the RIGHT button. This displays a dialog box.

For the Emissivity,‎ Temp unit,‎ and Auto off settings,‎ use the UP/DOWN buttons to go to the desired option.

For the Delete all and Restore actions,‎ use the LEFT/RIGHT buttons to select one of the following:

  • icon to execute the action.
  • icon to cancel the action.

Push the MID button to confirm and return to the Settings menu.

Push the LEFT button to return to the live image.