| WARNING | |
|
Applicability: Cameras with one or more laser pointers.
Do not look directly into the laser beam. The laser beam can cause eye irritation.
|
|
| WARNING | |
|
Make sure that you read all applicable MSDS (Material Safety Data Sheets) and warning labels on containers before you use
a liquid. The liquids can be dangerous. Injury to persons can occur.
|
|
| CAUTION | |
|
Do not point the infrared camera (with or without the lens cover) at strong energy sources, for example, devices that cause
laser radiation, or the sun. This can have an unwanted effect on the accuracy of the camera. It can also cause damage to
the detector in the camera.
|
|
| CAUTION | |
|
Do not use the camera in temperatures more than +50°C (+122°F), unless other information is specified in the user documentation
or technical data. High temperatures can cause damage to the camera.
|
|
| CAUTION | |
|
Do not apply solvents or equivalent liquids to the camera, the cables, or other items. Damage to the battery and injury
to persons can occur.
|
|
| CAUTION | |
|
Be careful when you clean the infrared lens. The lens has an anti-reflective coating which is easily damaged. Damage to the
infrared lens can occur.
|
|
| CAUTION | |
|
Do not use too much force to clean the infrared lens. This can cause damage to the anti-reflective coating. |
|
| Note | |
|
The encapsulation rating is only applicable when all the openings on the camera are sealed with their correct covers, hatches,
or caps. This includes the compartments for data storage, batteries, and connectors.
|
|