Follow this procedure:
Turn on the camera.
Connect the camera to the computer, using a USB cable.
Start the FLIR Report Studio wizard.
Select a report template and click Next at the bottom right of the window.

Click Import at the bottom left of the window.

The Import images dialog box is displayed, where you can see the images in the camera. For cameras with more than one folder, you can select the folders in the left pane.

In the right pane, select one or more of the check boxes:
Applicable to cameras with more than one folder. Do one of the following:

Applicable to cameras with one folder. Do one of the following:
The Browse For Folder dialog box is displayed. Select the destination folder or create a new folder.
The images are now imported to the computer.