|
|
WARNING |
|
Applicability: Class B digital devices.
This equipment has been tested and found to comply with the limits for a Class B digital device, pursuant to Part 15 of the
FCC Rules. These limits are designed to provide reasonable protection against harmful interference in a residential installation.
This equipment generates, uses and can radiate radio frequency energy and, if not installed and used in accordance with the
instructions, may cause harmful interference to radio communications. However, there is no guarantee that interference will
not occur in a particular installation. If this equipment does cause harmful interference to radio or television reception,
which can be determined by turning the equipment off and on, the user is encouraged to try to correct the interference by
one or more of the following measures:
|
|
|
|
WARNING |
|
Applicability: Digital devices subject to 15.19/RSS-GEN.
NOTICE: This device complies with Part 15 of the FCC Rules and with Industry Canada licence-exempt RSS standard(s). Operation is
subject to the following two conditions:
|
|
|
|
WARNING |
|
Applicability: Digital devices subject to 15.21.
NOTICE: Changes or modifications made to this equipment not expressly approved by FLIR Systems may void the FCC authorization to
operate this equipment.
|
|
|
|
WARNING |
|
Applicability: Digital devices subject to 2.1091/2.1093/KDB 447498/RSS-102.
Radiofrequency radiation exposure Information: The radiated output power of the device is far below the FCC radio frequency exposure limits. Nevertheless, the device should
be used in such a manner that the potential for human contact during normal operation is minimized.
|
|
|
|
WARNING |
|
This device is granted pursuant to the Japanese Radio Law (電波法) and the Japanese Telecommunications Business Law (電気通信事業法).
This device should not be modified (otherwise the granted designation number will become invalid)
|
|
|
|
WARNING |
|
Do not look directly into the laser beam. The laser beam can cause eye irritation.
|
|
|
|
WARNING |
|
Do not point the camera at the face of a person when the continuous autofocus function is on. The camera uses laser distance
measurements (that are continuous) for the focus adjustments. The laser beam can cause eye irritation.
|
|
|
|
WARNING |
|
Do not point the camera at the face of a person when you use the autofocus function. You can set the camera to use a laser
distance measurement for the focus adjustment. The laser beam can cause eye irritation.
|
|
|
|
WARNING |
|
Do not disassemble or do a modification to the battery. The battery contains safety and protection devices which, if damage
occurs, can cause the battery to become hot, or cause an explosion or an ignition.
|
|
|
|
WARNING |
|
If there is a leak from the battery and you get the fluid in your eyes, do not rub your eyes. Flush well with water and immediately
get medical care. The battery fluid can cause injury to your eyes if you do not do this.
|
|
|
|
WARNING |
|
Do not continue to charge the battery if it does not become charged in the specified charging time. If you continue to charge
the battery, it can become hot and cause an explosion or ignition. Injury to persons can occur.
|
|
|
|
WARNING |
|
Only use the correct equipment to remove the electrical power from the battery. If you do not use the correct equipment, you
can decrease the performance or the life cycle of the battery. If you do not use the correct equipment, an incorrect flow
of current to the battery can occur. This can cause the battery to become hot, or cause an explosion. Injury to persons can
occur.
|
|
|
|
WARNING |
|
Make sure that you read all applicable MSDS (Material Safety Data Sheets) and warning labels on containers before you use
a liquid. The liquids can be dangerous. Injury to persons can occur.
|
|
|
|
CAUTION |
|
Do not point the infrared camera (with or without the lens cover) at strong energy sources, for example, devices that cause
laser radiation, or the sun. This can have an unwanted effect on the accuracy of the camera. It can also cause damage to the
detector in the camera.
|
|
|
|
CAUTION |
|
Do not use the camera in temperatures more than 50°C (122°F), unless other information is specified in the user documentation or technical data. High temperatures can cause damage to
the camera.
|
|
|
|
CAUTION |
|
Do not attach the batteries directly to a car’s cigarette lighter socket, unless FLIR Systems supplies a specific adapter
to connect the batteries to a cigarette lighter socket. Damage to the batteries can occur.
|
|
|
|
CAUTION |
|
Do not connect the positive terminal and the negative terminal of the battery to each other with a metal object (such as wire).
Damage to the batteries can occur.
|
|
|
|
CAUTION |
|
Do not get water or salt water on the battery, or permit the battery to become wet. Damage to the batteries can occur.
|
|
|
|
CAUTION |
|
Do not make holes in the battery with objects. Damage to the battery can occur.
|
|
|
|
CAUTION |
|
Do not hit or cause shocks to the battery. Damage to the battery can occur.
|
|
|
|
CAUTION |
|
Do not put the batteries in or near a fire, or into direct sunlight. When the battery becomes hot, the built-in safety equipment
becomes energized and can stop the battery charging procedure. If the battery becomes hot, damage can occur to the safety
equipment and this can cause more heat, damage or ignition of the battery.
|
|
|
|
CAUTION |
|
Do not put the battery on or near fires, stoves, or other high-temperature locations. Damage to the battery and injury to
persons can occur.
|
|
|
|
CAUTION |
|
Do not solder directly onto the battery. Damage to the battery can occur.
|
|
|
|
CAUTION |
|
Do not use the battery if, when you use, charge, or put the battery in storage, there is an unusual smell from the battery,
the battery feels hot, changes color, changes shape, or is in an unusual condition. Speak with your sales office if one or
more of these problems occurs. Damage to the battery and injury to persons can occur.
|
|
|
|
CAUTION |
|
Only use a specified battery charger when you charge the battery. Damage to the battery can occur if you do not do this.
|
|
|
|
CAUTION |
|
Only use a specified battery for the camera. Damage to the camera and the battery can occur if you do not do this.
|
|
|
|
CAUTION |
|
The temperature range through which you can charge the battery is ±0°C to +45°C (+32°F to +113°F), except for the Korean market where the approved range is +10°C to + 45°C (+50°F to +113°F). If you charge the battery at temperatures out of this range, it can cause the battery to become hot or to break. It can
also decrease the performance or the life cycle of the battery.
|
|
|
|
CAUTION |
|
The temperature range through which you can remove the electrical power from the battery is -15°C to +50°C (+5°F to +122°F), unless other information is specified in the user documentation or technical data. If you operate the battery out of this
temperature range, it can decrease the performance or the life cycle of the battery.
|
|
|
|
CAUTION |
|
When the battery is worn, apply insulation to the terminals with adhesive tape or equivalent materials before you discard
it. Damage to the battery and injury to persons can occur if you do not do this.
|
|
|
|
CAUTION |
|
Remove any water or moisture on the battery before you install it. Damage to the battery can occur if you do not do this.
|
|
|
|
CAUTION |
|
Do not apply solvents or equivalent liquids to the camera, the cables, or other items. Damage to the battery and injury to
persons can occur.
|
|
|
|
CAUTION |
|
Be careful when you clean the infrared lens. The lens has an anti-reflective coating which is easily damaged. Damage to the
infrared lens can occur.
|
|
|
|
CAUTION |
|
Do not use too much force to clean the infrared lens. This can cause damage to the anti-reflective coating.
|
|
|
|
CAUTION |
|
Make sure that the beams from the intensive energy sources do not go into the viewfinder. The beams can cause damage to the
camera. This includes the devices that emit laser radiation, or the sun.
|
|
|
|
CAUTION |
|
Applicability: Camera with IR lens f=70 mm (6°)
When you hold the camera, make sure that you support the lens with your hand. The lens is heavy, and the joint between the
optics and camera housing is not strong enough to support the lens.
|
|
|
|
CAUTION |
|
The 5 GHz band is only allowed for indoor use in Japan and Canada.
|
|