28 Updating the camera
To take advantage of our latest camera firmware, it is important that you keep your camera updated.
28.1 Prepare for update Over-The-Air (OTA)
Camera update Over-The-Air (OTA) is a new feature.
If your camera has an earlier firmware version, you must first manually update the camera to the latest version before your
camera can be updated Over-The-Air (OTA).
To see which version is installed on your camera, select Settings > Device settings > Camera information > Software.
28.2 Update the camera Over-The-Air (OTA)
Note
If a new firmware version is available, there will be a notification on the Settings menu.
To install a new firmware version, do the following:
-
Make sure the camera battery is fully charged.
-
Make sure the camera has Wi-Fi enabled and is connected to the internet.
-
Select Settings > Device settings > Update.
-
If an update is available, select Download to download the installation package.
-
Select Install to start the installation.
-
When the installation is completed, the camera will automatically restart.
28.3 Update via USB cable with the FLIR Camera Updater
The FLIR Camera Updater is a Windows application used to update the camera.
To update your camera, you must log in to your FLIR account or sign up for a new account. You must also register the camera.
28.3.1 Install the FLIR Camera Updater
-
Go to
https://support.flir.com
. Find the software download area and search for FLIR Camera Updater.
-
Download the FLIR Camera Updater installer package.
-
Start the installation by double-clicking the executable installer file.
-
Follow the instructions in the setup wizard.
28.3.2 Connect the camera
-
Connect the camera to the computer, using the USB cable.
-
Turn on the camera.
-
Run the FLIR Camera Updater application.
-
Sign in to your FLIR account or sign up for a new account.
-
The application automatically connects to the camera.
-
If the camera is not registered, select Product registration and complete the registration.
-
If a newer firmware version is available, you can select to update the connected camera.
28.3.3 Update notifications
The FLIR Camera Updater can send notifications if there is a new update available for your previously connected devices.