6  Using the FLIR ONE‎ app

6.1  Camera view

When the FLIR Edge‎ camera is connected to the FLIR ONE‎ app, you can see the live view from the camera and take an image or record a video.
    The camera view contains functionality to modify the live view:
  • IR Scale: Hide/show scale. Adjust scale limits.
  • Color: Choose from nine color palettes.
  • Measurements: Adjustable measurement spots. Automatic tracking of hottest and coldest spot.
  • Image mode: Thermal, DC (visual), MSX.
  • MSX Distance: Align visual and thermal images in MSX mode, depending on distance to object.
  • Temperature range: Choose suitable object temperature range.

6.2  Calibration

The camera automatically calibrates and refreshes the image periodically to provide an optimal image. The thermal camera has a mechanical shutter inside that activates during calibration, which releases a clicking sound. When the shutter activates, the image will freeze for a brief period. When the camera first turns on, and periodically thereafter, the camera will automatically calibrate. It is also possible to manually initiate a calibration in the FLIR ONE‎ app.

6.3  Gallery

Captured images and videos can be viewed in the gallery of the FLIR ONE‎ app. Images and videos can also be saved in the gallery of the mobile device, if permission is given. Permissions are set during the initial setup, or later in the FLIR ONE‎ app settings.
Information related to the image is presented in Image details, where it is also possible to add a note to the image.
In the gallery of the FLIR ONE‎ app, images can be edited with the same functionality as in the camera view.
Images and videos can be shared with other apps, for example a social media app on your mobile device.
You can upload images and videos to cloud storage, see section 6.4 Cloud storage .

6.4  Cloud storage

FLIR Ignite‎ is a cloud storage service for thermal images. In FLIR Ignite‎, you can view, organize, search for, download, and share your uploaded images.
You can manually upload image and video files from the gallery of the FLIR ONE‎ app to your FLIR Ignite‎ account.
In your Ignite account settings, you can set the app to automatically upload files. There is also a setting to use mobile data to upload to FLIR Ignite‎. If this setting is turned off, you must disconnect the FLIR ONE‎ app from the FLIR Edge‎ camera and pair the app with a FLIR Ignite‎ account before you can upload files.
To create and access your FLIR Ignite‎ account, go to https://ignite.flir.com‎ .

6.5  Drawer menu

    In the drawer menu you find:
  • Settings and account information related to FLIR Ignite‎.
  • Information related to the camera.
  • Settings for the FLIR ONE‎ app.
  • Help on how to use the app.
  • Contact to support.
  • Other available apps that are compatible with the FLIR Edge‎ camera.