5  Introduction

The Smart Sensor and Image Streaming cameras of the FLIR A400/A500/A700 series offer unmatched power and flexibility to tailor effective thermal monitoring that improves quality, productivity, maintenance, and safety.
  • The Smart Sensor cameras analyze the images and then deliver a result to the user.
    Use Modbus TCP, Ethernet /IP, or ONVIF to integrate the cameras into industrial systems (HMI/SCADA, VMS, NVR), or use the REST API to transfer data from the camera to a web interface or to an application on the internet.
  • The Image Streaming cameras deliver images with all related information to a computer where the user can analyze the images and then decide what to do next.
    Use the GigE Vision and GeniCam compatibility to integrate the cameras into your own system.
Typical applications where the Smart Sensor and Image Streaming cameras of the FLIR A400/A500/A700 series can be used are:
  • Early fire detection
  • Quality assurance
  • Condition monitoring
For system installation examples, see 5.1 Example system overviews .

5.1  Example system overviews

5.1.1  Early fire detection

Graphic

Figure 5.1  Hot spot detection, self-combustible material on conveyor belt

Graphic

Figure 5.2  Hot spot detection, self-combustible material in storage areas

5.1.2  Quality assurance

Graphic

Figure 5.3  Checking hot glue on cardboard boxes

5.1.3  Condition monitoring

Graphic

Figure 5.4  24/7 monitoring of critical assets

5.1.4  Research & development

Graphic

Figure 5.5  Checking heat dissipation on PCB during development