9  Visitor — Screening procedure

This chapter focuses on the visitor and describes the screening procedure.

9.1  Remove your glasses

Removing eyeglasses is crucial for a correct screening result. If the system detects eyeglasses, a message is displayed.
Graphic
 

9.2  Too many people

The system can only screen one person at the time. If the system detects more than one face, a message is displayed.
Graphic
 

9.3  Temperature cannot be evaluated

The system only evaluates temperatures within a certain temperature range. If the measured temperature is outside this range, a message is displayed.
Graphic
Graphic

9.4  System closed

When the system is closed, a message is displayed.
Graphic