8  FLIR Ignite Sync‎

FLIR Ignite Sync is a PC–based (Windows 10) application that automatically syncs your FLIR Ignite Library with a sync folder on your computer.
You can add or rename images in your FLIR Ignite Library or in the sync folder on your computer and all of your changes will instantly be synced.

8.1  System requirements

    For automatic sync to work, the following is required:
  • FLIR Ignite Sync must be installed on your Windows 10 computer.
  • FLIR Ignite Sync must be running on your computer.
  • You must have logged in to your FLIR Ignite account via FLIR Ignite Sync.
  • Your computer must be connected to internet.

8.2  Installation and setup

8.3  Start application

When the application is running and you are logged in to your FLIR Ignite account, the FLIR Ignite Sync icon looks like this: Graphic .

8.4  User interface

To display the user interface, click Graphic in the taskbar.
Graphic