24  Cleaning the camera

24.1  Camera housing, cables, and other items

    Use one of these liquids:
  • Warm water
  • A weak detergent solution
    Equipment:
  • A soft cloth

Follow this procedure:

24.2  Infrared lens

    Use one of these liquids:
  • A commercial lens cleaning liquid with more than 30% isopropyl alcohol.
  • 96% ethyl alcohol (C2H5OH).
    Equipment:
  • Cotton wool

Follow this procedure:

24.3  Infrared detector

Even small amounts of dust on the infrared detector can result in major blemishes in the image. To remove any dust from the detector, follow the procedure below.