10  Working with the image archive

10.1  General

When you save an image or video clip, the camera stores the image/video file in the image archive on the memory card. You can open an image in the image archive and, for example, select another image mode, apply color alarms, and add measurement tools. You can also open and play saved video clips.
In the camera, the image archive is called Gallery. The Gallery can include one or several folders. New images and video clips will be saved to the active folder, at the top of the Gallery. You can create new folders, rename a folder, change the active folder, move files between the folders, and delete folders.

10.1.1  Managing folders via soft button

The soft button icon can be used to open a menu, where you can create new folders and change the active folder.

10.2  Opening image and video files

10.3  Creating a new folder

10.4  Renaming a folder

You can change the name of the folders in the archive. The active folder cannot be renamed.

To rename a folder, do the following:

10.5  Changing the active folder

New images and video clips are saved to the active folder.

To change the active folder, do the following:

10.6  Moving files between folders

10.7  Uploading files and folders

You can manually upload images, videos, and folders to your FLIR Ignite account when the camera is connected to the internet. For more information, see section 9.6 Manual upload .

10.8  Deleting a folder

You can delete a folder in the archive. The active folder cannot be deleted.

10.9  Deleting an image or video file

You can delete an image or video file from the image archive.

10.10  Deleting multiple files

You can delete multiple image and video files from the image archive.

10.11  Deleting all files

You can delete all image and video files from the memory card.