12  Working with image modes

12.1  General

The camera can capture both thermal and visual images at the same time. By choosing the image mode, you select which type of image to display on the screen.
The camera supports the following image modes:
  • Thermal: An infrared image is displayed.
  • Thermal MSX (Multi Spectral Dynamic Imaging): The camera displays an infrared image where the edges of the objects are enhanced with visual image details.
  • Picture in picture: An infrared image frame is displayed on top of the visual image.
  • Digital camera: The visual image captured by the digital camera is displayed.
  • Macro: This mode enables the camera to focus on objects very close to the camera lens. An infrared image is displayed.

12.2  Image examples

This table explains the different types of image modes.
Graphic
Thermal
Graphic
Thermal MSX
Graphic
Picture in picture
Graphic
Digital camera
Graphic
Macro
 

12.3  Selecting an image mode

Follow this procedure: