14  Working with color alarms and isotherms

14.1  Color alarms

By using color alarms (isotherms), anomalies can easily be discovered in an infrared image. The isotherm command applies a contrasting color to all pixels with a temperature above, below, or between the set temperature levels. The camera also features isotherm types that are specific to the building trade: condensation and insulation alarms.
You can make the camera trigger the following types of color alarms:
  • Above alarm: This will apply a contrasting color to all pixels with a temperature above the specified temperature level.
  • Below alarm: This will apply a contrasting color to all pixels with a temperature below the specified temperature level.
  • Interval alarm: This will apply a contrasting color to all pixels with a temperature between two specified temperature levels.
  • Condensation alarm: Triggers when the camera detects a surface where the relative humidity exceeds a preset value.
  • Insulation alarm: Triggers when there is an insulation deficiency in a wall.
This table explains the different color alarms (isotherms).
Graphic
Above alarm
Graphic
Below alarm
Graphic
Interval alarm
Graphic
Condensation alarm
Graphic
Insulation alarm
 

14.1.1  Setting up above, below, and interval alarms

14.1.2  Building isotherms

14.1.2.1  About the Condensation alarm

To detect areas with potential moisture problems, you can use the Condensation alarm. You can set the relative humidity above which the isotherm will colorize the image.

14.1.2.2  About the Insulation alarm

The Insulation alarm can detect areas where there may be an insulation deficiency in the building. It will trigger when the insulation level (which is called the thermal index in the camera) falls below a preset value of the energy leakage through a wall.
Different building codes recommend different values for the insulation level, but typical values are 60–80% for new buildings. Refer to your national building code for recommendations.

14.1.2.3  Setting up condensation and insulation alarms