1. This item is dependent on the lens model.
2. This item is dependent on the lens model.
3. This item is dependent on the lens model.
4. This item is dependent on the lens model.
5. Not supported when using macro.
6. Definition from the European standard EN 16714-3:2016, Non-destructive Testing—Thermographic Testing—Part 3: Terms and Definitions.
7. This item is dependent on the camera model.
8. Not supported when using macro.
9. http://www.bipm.org/en/about-us/ [Retrieved 2017-01-31.]
10. http://jcgm.bipm.org/vim/en/2.39.html [Retrieved 2017-01-31.]
11. http://jcgm.bipm.org/vim/en/4.30.html [Retrieved 2017-01-31.]
12. http://jcgm.bipm.org/vim/en/4.31.html [Retrieved 2017-01-31.]