Follow this procedure:
Before starting the camera for the first time, charge the battery for 3 hours using the stand-alone battery charger.
Put the battery into the camera battery compartment.
Insert a memory card into the card slot.
Push the on/off button
to turn on the camera.
Follow the instructions on the camera screen to configure your camera. You can, for example, select the language, units, and date and time formats.
You can also set up the camera to upload images for storage online. To enable upload of images, you need to connect the camera to the internet and pair the camera with a FLIR Ignite account. Use a computer or other device with internet access and follow the instructions on the camera screen.
To enable automatic upload of images, select
(Settings), sign in to FLIR Ignite, and set the Auto upload switch to On.
Aim the camera toward the object of interest.
Adjust the infrared camera focus.
Push the Save button to save an image.
If automatic upload is enabled, new images will automatically be uploaded to your FLIR Ignite account when the camera is connected to the internet. You can also upload images manually. To access your FLIR Ignite account, go to https://ignite.flir.com .
You can also move images from the camera using the USB cable or the memory card.
Import the images into a FLIR Thermography software and create an inspection report.