19  Screening alarm

The screening alarm can be used to detect temperature anomalies in a series of inspected objects in a similar/fixed setup.

19.1  General

The basics of the screening alarm is to first build up a base of reference temperature samples. When an object is screened, the camera compares the measured temperature with the average of the reference samples. If the camera detects a temperature that is above a specified threshold, an alarm will trigger.
Graphic
The camera detects and measures the temperature of the hottest spot within the measurement box.
An alarm will trigger when the measured temperature is higher than the alarm limit. The camera will also apply a red color to all parts of the image with a temperature above the alarm limit.
The alarm limit is the sum of a sampled average temperature and a specified allowed deviation.

19.2  Work flow

19.2.1  Activate and configure the screening alarm

19.2.2  Record reference samples

Before the screening can start, you must record reference samples. These are used to calculate the reference temperature average.
You record the reference samples by screening 10 inspection objects. Make sure these objects have a normal temperature.

19.2.3  Perform the screening