18  Inspection Route‎

18.1  General

FLIR Inspection Route is a solution that streamlines thermal inspections and simplifies data collection and reporting. The solution includes FLIR software and camera support for preparation, inspection, and post-processing.
With the Inspection Route function, the camera guides the operator along a predefined route of inspection points, where images and data are collected in a structured manner. FLIR Inspection Route speeds up post-processing and reporting by ensuring that nothing is missed and that all inspection results are organized right from the start.
The inspection work flow is defined by a Route file, with a high degree of flexibility. It is possible to configure an automated work flow, where the camera automatically sets the status and steps to the next inspection point when an image is saved. The operator can also manually select the status, add comments, and add more images.
The Route file is used as template when starting an inspection in the camera. It is possible to have multiple Route files in camera and the operator can run multiple inspections based on any of the Route files in the camera.
Reference images provide aiming support, increase quality in decision making in the field, and speeds up data collection by defining a baseline for the user based on a set of predefined parameters.

18.1.1  Work flow

18.1.2  FLIR Inspection Route‎ Solution user manual

The FLIR Inspection Route Solution user manual describes how to configure Route files, perform inspections, transfer inspection results, and create inspection reports using a camera with FLIR Inspection Route enabled, the FLIR Thermal Studio application, and the FLIR Ignite cloud service.
To access the FLIR Inspection Route Solution user manual, go to http://support.flir.com/resources/route .

18.1.3  First generation FLIR Inspection Route‎

The first generation of the Inspection Route functionality in the camera was based on an inspection route file in .xml format. The new Inspection Route functionality is based on a Route file in .routex format.
The camera still supports the xml based functionality. However, it is not possible to use a mix of .xml and .routex files on the camera memory card.
If there is an inspection route file (.xml) at the root of the memory card, the camera will start an inspection based on the .xml file when you activate the Inspection Route functionality.

18.1.3.1  User manual

For a description of the xml based FLIR Inspection Route functionality, refer to the user manual for the FLIR Inspection Route Solution, First generation.
To access the user manual, go to http://support.flir.com/resources/route.

18.2  Route file

The Route file specifies the structure, consisting of multiple levels of locations, assets, and inspection points. The Route file also specifies the available statuses and the configuration of the camera behavior and includes any reference images.
You can create the Route files in FLIR Thermal Studio.
The Route files must be placed in a folder named Routes located at the root of the camera memory card.

18.3  Inspection file

You can start a new inspection based on any of the Route files available in the Routes folder on the camera memory card.
During the inspection, the camera stores the inspection results internally. When you pause, finish, upload, or deactivate the Inspection Route function, the camera creates a package — an Inspection file (.route) — that includes all the inspection data (status, comments) and images for each inspection point.
The camera stores the Inspection file (.route) in a folder named Inspections located at the root of the memory card.

18.4  User interface

Graphic
The Inspection Route overlay consists of the following parts:
  • Back arrow
    Tap to go to the previous inspection point.
  • Current point indicator
    • Displays the name of the current inspection point.
    • Displays an image icon if there is an image saved for the inspection point.
    • Displays the status of the inspection point.
  • Next arrow
    Tap to go to the next inspection point.
  • Document icon
    This icon is displayed if there is a description and/or comment available for the inspection point. A description comes from the Route file and can, for example, include instructions or reminders for the inspection point. Comments are text notes added during the inspection. Tap the icon to display the description and/or comment.
  • Reference image

18.4.1  Reference image

You can use the reference image for aiming support. It is possible to switch between the infrared and visual reference image.
When maximized, the reference image covers the entire screen.
With the Overlay functionality enabled, the reference image is transparent and is displayed over the live image.
Graphic

18.4.2  Drop-down menu

To display the drop-down menu, tap the current point indicator.
Graphic
In the drop-down menu it is possible to:
  • Set the status of the current inspection point.
  • View the filenames of images saved for this inspection point.
  • Add comments for the current inspection point.
  • Open the inspection list, see section 18.5.8 Inspection list .

18.5  Perform inspection

This procedure assumes that one or more Route files (.routex) have been created.

18.5.1  General

To perform an inspection, you first have to add one or more Route files to the camera memory card. The Route files must be placed in a folder named Routes located at the root of the camera memory card. See also section 18.2 Route file .
You can start a new inspection based on any of the Route files available on the camera memory card. During the inspection, the camera stores the inspection results internally. When the inspection is completed, the camera creates an Inspection file with the inspection results and stores the file in a folder named Inspections located at the root of the memory card. See also section 18.3 Inspection file .
When uploading the inspection results to FLIR Ignite, the camera uploads the Inspection file (.route) to your FLIR Ignite account. Uploading the Inspection file (.route) does not remove the file from the Inspections folder located at the root of the memory card.

18.5.2  Add the Route file to the memory card

18.5.3  Inspection settings

18.5.3.1  Route file settings

The behavior of the camera during the inspection is controlled via settings in the Route file. It is also possible to define these settings in the camera, see section 18.6 Configuration .
To use the settings from the Route file, select Settings > Routing > Inspection settings > Use Route settings = On.

18.5.3.2  Reference image settings

The camera can be configured to use the settings and parameters from the reference image. For more information, see section 18.7 Use settings and parameters from reference images .
To use the settings and parameters from the reference images, select Settings > Routing > Inspection settings > Reference image > Apply parameters = On.

18.5.4  Start an inspection

18.5.5  Capture inspection data

18.5.6  Save an image

When you take an image, the camera automatically saves the image to the memory card.
You can take and save multiple images of the inspection point.

18.5.7  Inspection images

During the inspection, the camera saves the inspection images to the memory card. While an inspection is ongoing, the images are also available in the image archive.
When you pause, finish, upload, or deactivate the Inspection Route function, the camera adds all inspection images to the Inspection file (.route) and the images are no longer available in the image archive. You can always open an Inspection from the Settings menu and view the images via the Inspection list, see section 18.5.8 Inspection list .

18.5.8  Inspection list

In the inspection list, you can see the progress of the inspection and review the inspection point results.
The content of the inspection list is defined by the Route file. The route structure and names come from the file.

18.5.9  Edit inspection point data

You can edit the data for the inspection point displayed by the current point indicator.
To go to another inspection point, use the back or next arrow or select the inspection point from the inspection list, see section 18.5.8 Inspection list .

18.5.9.1  Set the status

18.5.9.2  Delete an image

18.5.9.3  Add a comment

18.5.10  Record a video clip

You can record and save video clips of the inspection point. For more information, see section 17 Recording video clips .

18.5.11  Transfer inspection results

You can upload the inspection results to your FLIR Ignite account or transfer the result files manually using the USB cable or the memory card.

18.5.11.1  Upload results to FLIR Ignite‎

18.5.11.2  Move results manually

18.6  Configuration

The behavior of the camera during the inspection is controlled via settings in the Route file. It is possible to override the Route settings and define the settings in the camera.
To define the camera behavior settings in the camera, do the following:

18.7  Use settings and parameters from reference images

The camera can be configured to use the settings and parameters from the reference images. At each inspection point, the camera will automatically apply the same measurement tools, measurement parameters (e.g. emissivity, reflected temperature, etc.), temperature scale values, and color palette as in the reference image.