Follow this procedure:
Do one of the following:
Follow this procedure:
Do one of the following:
Follow this procedure:
On the measurement toolbar, select
(Rotate image and measurements). This displays a toolbar.
On the toolbar, do one of the following:
Follow this procedure:
On the measurement toolbar, select
(Crop). This displays a box on the image.
Select the crop region by moving and adjusting the size of the box.
In the crop region box, do one of the following:
Follow this procedure:
On the measurement toolbar, select one of the following:
Click the location on the image where the measurement tool is to be placed.
Follow this procedure:
On the measurement toolbar, select
(Selection).
To move a measurement tool, select the tool on the image and drag it to a new position.
To resize a measurement tool, select the tool on the image and use the selection tool to drag the handles that are displayed around the frame of the tool.

Follow this procedure:
Add one or several line tools to the image, see section 11.5.2 Adding a measurement tool .
Click the Profile tab. This displays the profile plot in the right pane.

In the right pane, you can select the following types of temperature scales for the plot:
In the right pane, select the
check box to reverse the start and end points of the line.
Follow this procedure:
On the measurement toolbar, select
(Selection).
Right-click the tool and select Local max/min/avg markers.
In the dialog box, select or clear the markers you want to add or remove.
Click OK.
Follow this procedure:
Add a box or circle measurement tool, see section 11.5.2 Adding a measurement tool .
Adjust the size of the box or circle tool to the size of the object, see section 11.5.3 Moving and resizing a measurement tool .
Right-click the tool and select Local max/min/avg markers. In the dialog box, select the Area check box. This displays the calculated area, based on the distance value, in the MEASUREMENTS pane.
To change the distance value, click the value field in the PARAMETERS pane, type a new value and press Enter. The recalculated area, based on the new distance value, is displayed in the MEASUREMENTS pane.
Follow this procedure:
Add a line measurement tool, see section 11.5.2 Adding a measurement tool .
Adjust the size of the line tool to the size of the object, see section 11.5.3 Moving and resizing a measurement tool .
Right-click the tool and select Local max/min/avg markers. In the dialog box, select the Length check box. This displays the calculated length, based on the distance value, in the MEASUREMENTS pane.
To change the distance value, click the value field in the PARAMETERS pane, type a new value and press Enter. The recalculated area, based on the new distance value, is displayed in the MEASUREMENTS pane.
Follow this procedure:
On the measurement toolbar, select
(Add delta).
The difference calculation is displayed under MEASUREMENTS in the right pane.

To change the setup for the difference calculation, do the following:
To delete the difference calculation, click
(Delete).
Follow this procedure:
On the measurement toolbar, select
(Selection).
Select the measurement tool on the image and do one of the following:
Automatic
|
Manual
|
Automatic
|
Manual
|
Follow this procedure:
To change the top level in the temperature scale, drag the top slider up or down.
To change the bottom level in the temperature scale, drag the bottom slider up or down.
Follow this procedure:
To auto-adjust the image, click Auto.
Follow this procedure:
On the measurement toolbar, select
(Set auto adjust region).
Use the displayed tool to create a region. This region can be moved and resized to suit your area of interest.

To delete the auto-adjust area, select the region and do one of the following:
Follow this procedure:
Right-click the image and select Color distribution. This displays a menu.
On the menu, select one of the following:
|
Color palette |
Image example |
|---|---|
|
Artic
|
|
|
Cool
|
|
|
Gray
|
|
|
Iron
|
|
|
Lava
|
|
|
Rainbow
|
|
|
Rainbow HC
|
|
|
Warm
|
|
Follow this procedure:
On the measurement toolbar, select
(Color). This displays a menu.
On the menu, click the palette you want to use.
|
Image mode |
Image example |
|---|---|
|
Thermal MSX (Multi Spectral Dynamic Imaging): This mode displays an infrared image where the edges of the objects are enhanced. The thermal/photo
balance can be adjusted.
|
|
|
Thermal: This mode displays a fully infrared image.
|
|
|
Thermal Fusion: This mode displays a digital photo where some parts are displayed in infrared, depending on the temperature limits.
|
|
|
Thermal Blending: The camera displays a blended image that uses a mix of infrared pixels and digital photo pixels. The thermal/photo balance
can be adjusted.
|
|
|
Picture in picture: This mode displays an infrared image frame on top of a digital photo.
|
|
|
Digital camera: This mode displays a fully digital photo.
|
|
Follow this procedure:
On the image mode toolbar, select one of the following:
Applicable to the Thermal MSX and Thermal Blending modes: To adjust the thermal/photo balance, click the arrow next to the image mode icon and drag the slider left or right.
Applicable to the Digital camera mode: To change the image to grayscale, click the arrow next to the image mode icon and select the check box.
|
Color alarm |
Image |
|---|---|
|
Above alarm
|
|
|
Below alarm
|
|
|
Interval alarm
|
|
|
Humidity alarm
|
|
|
Insulation alarm
|
|
Follow this procedure:
On the measurement toolbar, select
(Color). This displays a menu.
On the menu, select one of the following:
In the right pane, take note of the parameter Limit . Areas in the image with a temperature above or below this temperature will be colorized with the isotherm color. You can change this limit, and also change the isotherm color on the Color menu.
Follow this procedure:
On the measurement toolbar, select
(Color). This displays a menu.
On the menu, select Interval alarm.
In the right pane, take note of the parameters Upper limit and Lower limit . Areas in the image with a temperature between these two temperatures will be colorized with the isotherm color. You can change these limits, and also change the isotherm color on the Color menu.
Follow this procedure:
On the measurement toolbar, select
(Color). This displays a menu.
On the menu, select Humidity alarm. Depending on your object, certain areas will now be colorized with an isotherm color.
In the right pane, take note of the parameter Calculated limit . This is the temperature at which there is a risk of humidity. If the parameter Relative humidity limit is set to 100%, this is also the dew point, i.e., the temperature at which the humidity falls out as liquid water.
Follow this procedure:
On the measurement toolbar, select
(Color). This displays a menu.
On the menu, select Insulation alarm. Depending on your object, certain areas will now be colorized with an isotherm color.
In the right pane, take note of the parameter Calculated insulation . This is the temperature where the insulation level falls below a preset value of the energy leakage through the building structure.
Follow this procedure:
On the measurement toolbar, select
(Color). This displays a menu.
On the menu, select Custom alarm.
In the right pane, specify the following parameters:
Follow this procedure:
On the measurement toolbar, select
(Selection).
Right-click the tool and select Local parameters.
In the dialog box, select Use local parameters.
Enter a value for one or more parameters.
Click OK.
Follow this procedure:
Under TEXT ANNOTATIONS in the right pane, do one of the following:
Enter the desired labels and values. See the image below for examples.