12  Working in the Microsoft Word‎ environment

12.1  FLIR Word Add-in‎ screen elements

12.1.1  FLIR tab

After installation of FLIR Report Studio, the FLIR tab appears to the right of the standard tabs in the ribbon of your Microsoft Word documents.
Graphic

12.1.2  Settings menu

The Settings menu includes the following commands:
  • Update page numbers. Click to update the page numbers for fields related to images.
  • Set units. Click to set the preferred temperature and distance units. For more information, see section 12.9 Changing the settings .
  • Select language. Click to select the language. For more information, see section 12.9 Changing the settings .
  • Template categories. (Available when creating a report template.) Click to select a category for the report template. For more information, see section 13.2.5 Selecting a template category .
  • Help. Click to display the Help menu, see section 12.1.2.1 Help menu .

12.1.2.1  Help menu

The Help includes the following commands:
  • Documentation. Click and select Online to view the latest help files from the internet or Offline to view the help files that are installed on your computer.
  • FLIR Store. Click to go to the FLIR Store website.
  • FLIR support Center. Click to go to the FLIR Support Center.
  • License information. Click to display the License Viewer.
  • Check for updates. Click to check for software updates. For more information, see section 15 Software update .
  • About. Click to display the current version of the FLIR Word Add-in.

12.2  Managing objects in the report

12.2.1   General

A report template contains placeholders for objects such as thermal images, digital photos, tables, report properties, etc.
When you create a report based on a report template, these placeholders are automatically populated based on the images you choose to include in the report. You can also insert additional objects and modify their properties after you have launched the report in Microsoft Word, as described in the sections below.
When you create your own report templates, see section 13 Creating report templates , you insert objects and define their properties according to the sections below.

12.2.2  Inserting a thermal image object

A thermal image object is a placeholder that automatically loads a thermal image when a report is created.

Follow this procedure:

12.2.3  Inserting a digital image object

A digital image object is a placeholder for the visual image associated with a thermal image.

Follow this procedure:

12.2.4  Inserting a profile object

12.2.4.1   General

A profile object displays a profile plot for a line tool added to the associated thermal image. The profile plot shows how the temperature results vary over the line tool.

12.2.4.2   Procedure

Follow this procedure:

12.2.5  Inserting a field object

12.2.5.1   General

A field object is a placeholder that automatically displays information associated with a thermal image when a report is created.
A field object consists of a label and a value, e.g., Bx1 Average 42.3 ℃ . You can choose to display only the value in the report, e.g., 42.3 ℃ .

12.2.5.2   Procedure

Follow this procedure:

12.2.6  Inserting a table object

12.2.6.1   General

A table object is a placeholder that automatically displays a table with certain information associated with a thermal image when a report is created.
The following table objects are available:
  • Measurements.
  • Parameters.
  • METERLiNK.
  • Geolocation.
  • Camera Info.
  • File Info.
  • Text Annotations.
  • Notes.
  • Formulas.
In addition to the built-in table objects, you can create your own table objects. For more information, see section 12.2.6.3 Creating a custom table object .
You can also insert a summary table, including information about all thermal images in the report. For more information, see section 12.2.6.4 Inserting a summary table .

12.2.6.2  Inserting a table object

Follow this procedure:

12.2.6.3  Creating a custom table object

If the built-in table objects do not meet your needs, you can create your own table objects.

Follow this procedure:

12.2.6.4  Inserting a summary table

A summary table object is a placeholder that automatically displays a table with certain information on all of the thermal images in the report.

Follow this procedure:

12.2.7  Inserting a report properties object

A report properties object is a placeholder that automatically displays customer information and information about the inspection when a report is created.

Follow this procedure:

12.2.8  Resizing objects

12.2.8.1  Resizing an image or profile object

Follow this procedure:

12.2.8.2  Resizing a table object

Follow this procedure:

12.2.9  Replacing an image

You can replace an image in the report, while keeping all connections to other objects.

Follow this procedure:

12.2.10  Deleting objects

12.2.10.1  Deleting an image or profile object

Follow this procedure:

12.2.10.2  Deleting a field object

Follow this procedure:

12.2.10.3  Deleting a table object

Follow this procedure:

12.3  Editing an image

You can edit thermal images directly from the report using the FLIR Report Studio Image Editor.

Follow this procedure:

12.4  Working with formulas

12.4.1   General

The FLIR Word Add-in allows you to carry out advanced calculations on various items in the infrared image. A formula can contain all common mathematical operators and functions (+, –, ×, ÷, etc). Also, numerical constants such as π can be used.
Most importantly, references to measurement results, other formulas, and other numerical data can be inserted into formulas.
The formulas you create will be available in the FLIR Word Add-in and can be inserted in field and table objects in future reports.
You can export a formula to a text file. This text file can, for example, be sent to another computer and will after import be available in the FLIR Word Add-in on that computer. For more information, see section 12.4.4 Exporting and importing formulas .
  • A formula can operate only on a single infrared image: it cannot calculate, for example, differences between two infrared images.
  • You can use any existing METERLiNK data in the infrared image as a value in a formula, in the same way as you would use an infrared measurement value. METERLiNK data can be stored in the infrared image by using an external FLIR/Extech meter—such as a clamp meter or a moisture meter—together with the infrared camera.

12.4.2  Creating a simple formula

Creating a formula that calculates the temperature difference between two spots

12.4.3  Creating a conditional formula

For some applications, you may, for example, want to display the result of a calculation in a green font color if the result is lower than a critical value, and in a red font color if the result is higher than the critical value. You do this by creating a conditional formula using the IF statement.
The procedure below describes how you set up a conditional formula that displays the result from a temperature difference formula in red if the value is higher than 2.0 degrees, and in green if the value is lower than 2.0 degrees.

Creating a conditional formula using the IF statement

12.4.4  Exporting and importing formulas

You can export one or more formulas to a text file. This text file can, for example, be sent to another computer and then be imported to the FLIR Word Add-in on that computer.

12.5  Document properties

12.5.1   General

When creating an infrared report, the FLIR program extracts the Microsoft Word document properties for the report template and inserts these properties into corresponding Microsoft Word fields in the final report.
You can use these document properties to automate several time-consuming tasks when creating a report. For example, you may want to automatically add information such as the name, address, and e-mail address of the inspection site, the model name of the camera that you are using, and your e-mail address.

12.5.2  Types of document properties

There are two different types of document properties:
  • Summary document properties.
  • Custom document properties.
For the former, you can only change the values, but for the latter you can change both the labels and the values.

12.5.3  Creating and editing Microsoft Word‎ document properties

Creating and editing document properties

12.6  Creating a report

You can easily and efficiently create an infrared report using the FLIR Report Studio wizard.

Follow this procedure:

12.7  Exporting a report

Before you send the infrared report to your client, you can export it in one of the following formats:
  • Flat DocX: This exports the report as a flat report with the suffix “_flat”. A flat report can still be edited using ordinary Microsoft Word features, but it is no longer possible to manage the image, field, and table objects.
  • PDF: This exports the report as a non-editable PDF report.

Follow this procedure:

12.8  Creating a report template

You can create your own report templates using the FLIR Report Studio Template Editor.

Follow this procedure:

12.9  Changing the settings

You can change the units and language settings.

Follow this procedure:

12.10  Help menu

The Help menu includes links to support and training sources, license information, check for updates, etc.
The Help menu is available on the FLIR tab under Settings.