Follow this procedure:
Push the navigation pad to display the menu system.
Select
(Settings) and push the navigation pad. This displays the Settings menu.
Use the navigation pad to select Connections > Bluetooth .
Make sure Bluetooth is enabled by toggling the Bluetooth switch.
Select Available devices and push the navigation pad.
Wait until a list of available Bluetooth devices is displayed.
When a Bluetooth device is found, select the device to add it, and begin the pairing procedure. The device is then ready to be used.