To add a spot measurement tool, follow this procedure:
On the toolbar and in the Measurement tools section, click Spot.
In the image, click to insert the spot. The tool is labeled with a number, and it is also displayed in the Active measurements section.
To move the tool, click and hold the tool label in the image, and then move it into position.
To configure Settings for the tool, click
next to the tool in the Active measurements section. This displays the Settings dialog box.
To associate an alarm with the tool, see section 10.4.2 Working with alarms .
To remove the tool, click Settings
next to the tool in the Active measurements section, and then click Delete measurement.
To add a box measurement tool, follow this procedure:
On the toolbar and in the Measurement tools section, click Box.
In the image, click and then draw a box of a desired size. The tool is labeled with a number, and it is also displayed in the Active measurements section.
To move the tool, click and hold the tool label in the image, and then move it into position.
To resize the tool, click and hold one of the corners of the box in the image, and then move it to the desired size and shape.
To configure Settings for the tool, click
next to the tool in the Active measurements section. This displays the Settings dialog box.
To associate an alarm with the tool, see section 10.4.2 Working with alarms .
To remove the tool, click Settings
next to the tool in the Active measurements section, and then click Delete measurement.
To add a measurement mask tool, follow this procedure:
On the toolbar and in the Measurement tools section, click Measurement mask.
In the image, click to insert the starting point of the mask. Move the pointer and click to insert the next point. Continue until you have the captured the desired shape. Finish by clicking the starting point. The tool is labeled with a number, and it is also displayed in the Active measurements section.
To configure Settings for the tool, click
next to the tool in the Active measurements section. This displays the Settings dialog box.
To associate an alarm with the tool, see section 10.4.2 Working with alarms .
To remove the tool, click Settings
next to the tool in the Active measurements section, and then click Delete measurement.
To add a line measurement tool, follow this procedure:
On the toolbar and in the Measurement tools section, click Line.
In the image, click a starting point and then draw the line to the desired length. The tool is labeled with a number, and it is also displayed in the Active measurements section.
To move the tool, click and hold the tool label in the image, and then move it into position.
To change the length of the tool, click one of the end points, and then move it to the desired length.
To configure Settings for the tool, click
next to the tool in the Active measurements section. This displays the Settings dialog box.
To associate an alarm with the tool, see section 10.4.2 Working with alarms .
To remove the tool, click Settings
next to the tool in the Active measurements section, and then click Delete measurement.
To add a polyline measurement tool, follow this procedure:
On the toolbar and in the Measurement tools section, click Polyline.
In the image, click to insert the starting point of the polyline. Move the pointer and click to insert the next point. Continue until you have the desired shape. Finish by clicking Confirm. The tool is labeled with a number, and it is also displayed in the Active measurements section.
To move the tool, click and hold the tool label in the image, and then move it into position.
To configure Settings for the tool, click
next to the tool in the Active measurements section. This displays the Settings dialog box.
To associate an alarm with the tool, see section 10.4.2 Working with alarms .
To remove the tool, click Settings
next to the tool in the Active measurements section, and then click Delete measurement.
To add a delta measurement tool, follow this procedure:
On the toolbar and in the Measurement tools section, click Delta. The tool is displayed in the Active measurements section.
In the Active measurements section, click Settings
. The Delta settings dialog box appears.
To change the label of the tool, change the Delta name.
In the Variable 1 and Variable 2 lists, select the measurement results you want to use in the calculation.
Click Save changes.
To add a reference temperature, follow this procedure:
On the toolbar and in the Measurement tools section, click Reference temperature. The tool is displayed in the Active measurements section.
In the Active measurements section, click Settings
. The Reference temperature dialog box appears.
To change the label, change the Reftemp name.
In the Value box, type the temperature to be used as reference.
Click Save changes.
To configure an alarm based on the measurement result from a spot, box, or delta measurement tool, follow this procedure:
In the Active Measurements section, click the plus sign under Add alarm next to the measurement result to be used for the alarm. The Add alarm dialog box appears.
In the Alarm label section, type an Alarm name.
In the Trigger section, select the Condition and temperatures that will trigger this alarm:
|
Triggers an alarm when the temperature is above the specified Threshold value. Also type a Hysteresis value.
|
|
Triggers an alarm when the temperature is within the specified Min value and Max value.
|
Hysteresis is the interval within which the temperature value is allowed to vary without causing a change in the trigger. If the threshold is set above 30.0°C and the hysteresis is set at 2.0°C, the trigger goes high when the temperature rises above 30.0°C and stays high until the temperature drops below 28.0°C. In contrast, if the threshold is set below 30.0°C, and the same hysteresis value is kept, the trigger goes high if the temperature drops below 30.0°C and stays high until the temperature rises above 32.0°C.
In the Threshold time box, type the amount of time that has to pass before an alarm is triggered. This can be used to avoid false alarms.
In the Action section, select which actions the camera will perform when an alarm is triggered:
|
Automatically sends the captured Image, Result, or Video to the recipients defined in Settings > Alarm recipients. For more information, see section
10.6.2 Alarm recipients
.
|
|
Automatically sends the captured Image or Video to the FTP site defined in Settings > Alarm recipients. For more information, see section
10.6.2 Alarm recipients
.
|
|
Automatically saves the captured Image or Video to the memory of the camera.
|
|
Temporarily disables the periodic calibration while the image/video is being captured.
|
The image/video can later be viewed and managed under the Library tab:
When completed, click Set alarm. The alarm is now listed under Active alarms.
To configure an alarm based on the digital input, follow this procedure:
In the Active Measurements section, click the plus sign under Add alarm next to the digital input result to be used for the alarm. The Alarm dialog box appears.
In the Alarm label section, type an Alarm name.
In the Trigger section and in the Value list; select “0” to trigger the alarm on a low signal or select “1” to trigger on a high signal.
In the Action section, select which actions the camera will perform when an alarm is triggered:
|
Automatically sends the captured Image, Result, or Video to the recipients defined in Settings > Alarm recipients. For more information, see section
10.6.2 Alarm recipients
.
|
|
Automatically sends the captured Image or Video to the FTP site defined in Settings > Alarm recipients. For more information, see section
10.6.2 Alarm recipients
.
|
|
Automatically saves the captured Image or Video to the memory of the camera.
|
|
Temporarily disables the periodic calibration while the image/video is being captured.
|
The image/video can later be viewed and managed under the Library tab:
When completed, click Set alarm. The alarm is now listed under Active alarms.
The internal temperature sensor can act as a thermometer for the ambient temperature. To configure an alarm based on the internal temperature sensor, follow this procedure:
In the Active Measurements section, click the plus sign under Add alarm next to the Sensor temperature. The Alarm dialog box appears.
In the Alarm label section, type an Alarm name.
In the Trigger section, select the Condition and temperatures that will trigger this alarm:
|
Triggers an alarm when the temperature is above the specified Threshold value. Also type a Hysteresis value.
|
|
Triggers an alarm when the temperature is within the specified Min value and Max value.
|
Hysteresis is the interval within which the temperature value is allowed to vary without causing a change in the trigger. If the threshold is set above 30.0°C and the hysteresis is set at 2.0°C, the trigger goes high when the temperature rises above 30.0°C and stays high until the temperature drops below 28.0°C. In contrast, if the threshold is set below 30.0°C, and the same hysteresis value is kept, the trigger goes high if the temperature drops below 30.0°C and stays high until the temperature rises above 32.0°C.
In the Threshold time box, type the amount of time that has to pass before an alarm is triggered. This can be used to avoid false alarms.
In the Action section, select which actions the camera will perform when an alarm is triggered:
|
Automatically sends the captured Image, Result, or Video to the recipients defined in Settings > Alarm recipients. For more information, see section
10.6.2 Alarm recipients
.
|
|
Automatically sends the captured Image or Video to the FTP site defined in Settings > Alarm recipients. For more information, see section
10.6.2 Alarm recipients
.
|
|
Automatically saves the captured Image or Video to the memory of the camera.
|
|
Temporarily disables the periodic calibration while the image/video is being captured.
|
The image/video can later be viewed and managed under the Library tab:
When completed, click Set alarm. The alarm is now listed under Active alarms.
To change the global parameters, follow this procedure:
In the bottom right corner of the screen, click to select the parameter to change.
Change the parameter to the desired value, and then press Enter or click anywhere on the screen.
To reset the global parameters to the default values provided by FLIR, click Reset.
In the Active measurements section, click Settings
next to the tool for which you want to change the parameters. The Settings dialog box appears.
To activate the use of local parameters, select the Local parameters check box. The values for the Emissivity, Reflected temperature, and Distance parameters are now editable.
To deactivate the use of local parameters, deselect the Local parameters check box.
When completed, click Save changes.
On the toolbar and in the Data presentation modes section, click Image mode.
Select one of the available image modes.
To change the palette, follow this procedure:
On the toolbar and in the Data presentation modes, click Palette.
Select one of the available palettes.
To configure an isotherm, follow this procedure:
On the toolbar and in the Data presentation modes section, click Isotherm.
Select one of the available isotherms.
When a color alarm is selected, it is displayed in the Active measurements section. Also, a temperature indicator is added to the left side of the temperature scale located to the right of the image.
To change the threshold temperature, click Settings
next to the isotherm in the Active measurements section. The Settings dialog box appears.
In the Range section, set the threshold temperature of the isotherm:
Optionally, change the contrasting color in the Highlight color section.
When completed, click Save changes.
To configure an auto-adjust region, follow this procedure:
On the toolbar and in the Data presentation modes section, click Auto-adjust region.
In the image, click and then draw a region of a desired size.
To move the region, click and hold the region label in the image, and then move it into position.
To resize the region, click and hold one of the corners of the region in the image, and then move it to the desired size and shape.
To remove the region, click X in the region label.
To set the automatic calibration, follow this procedure:
On the toolbar and in the Calibration tools section, click Calibration. This displays a list of calibration options.
Click one of the options:
|
when needed.
|
|
approximately every 10 minutes, or when needed.
|
|
approximately every 30 minutes, or when needed.
|
|
approximately every 60 minutes, or when needed.
|
|
at any set interval.
|
|
never (automatic calibration disabled).
|
While the automatic calibration is in progress, the Notification text Calibration in progress ... is temporarily displayed under the live image.
To perform a manual calibration, follow this procedure:
On the toolbar and in the Calibration tools section, click Calibration. This displays a list of calibration options.
Click Calibrate now.
While the manual calibration is in progress, the Notification text Calibration in progress ... is temporarily displayed under the image on the screen
On the toolbar and in the Calibration tools section, click Light.
Click ON or OFF.
To change the maximum temperature level, type the temperature in the upper temperature scale box. As an alternative, click and hold the upper temperature bar on the scale, and then move it into position. Watch the temperature in the scale box change as you move the bar.
To change the minimum temperature level, type the temperature in the lower temperature scale box.As an alternative, click and hold the lower temperature bar on the scale, and then move it into position. Watch the temperature in the scale box change as you move the bar.
To return to auto-adjustment, click the Auto button(s).
On the toolbar and in the View modes section, click
to flip the image horizontally or click
to flip the image vertically.
To view the image in full screen, follow this procedure:
On the toolbar and in the View modes section, click Full screen.
To return to normal view, press the Esc (Escape) key on the computer keyboard.
To take a snapshot, follow this procedure:
On the toolbar and in the View modes section, click Snapshot.
The Notification text Snapshot stored is temporarily displayed under the live image.
To pause or freeze the live image stream, follow this procedure:
On the toolbar and in the View modes section, click Freeze.
To resume the live image stream, click Unfreeze.
To hide all overlay graphics in the live image, follow this procedure:
On the toolbar and in the View modes section, click Hide overlay.
To show any hidden overlay graphics, click Show overlay.
To save the current camera setup, follow this procedure:
In the Active measurements section, click Save preset.
To load a saved preset file, follow this procedure:
In the Active measurements section, click Load preset. The standard Windows Open dialog box appears.
Browse to the Downloads folder (or to the folder where you have stored the preset files).
Select the file, and then click Open. This loads and applies the presets.
In the navigation pane, click Network settings.
Select one of the following:
Click Apply.
In the navigation pane, click Network settings.
Click Server mode.
Type a Network name and a Password for accessing the network.
Click Share network.
The camera will now act as a “hotspot” that computers or tablets (with high resolution) can connect to. When a wireless connection
has been established, the camera will be available at the IP address 192.168.16.1.
In the navigation pane, click Network settings.
Click Client mode.
Click Scan networks.
Select one of the Available networks in the list, and then click Connect.
Type the Password for accessing the network, and then click Connect.
In the navigation pane, click Network settings.
In the Streaming bit rate list, select one of the available bit rates.
Click Apply.
In the navigation pane, click Alarm recipients.
In the Alarm recipient e-mail box, type the e-mail address of the recipient.
In the Mail server setup box, type the IP address of the sending mail server.
If the sending mail server requires a login (mail server authentication), select the Authentication required check box, and then type the credentials in the User and Password boxes.
Click Apply.
In the navigation pane, click Alarm recipients.
In the FTP Server IP address box, type the IP address of the FTP server.
In the Folder box, type the path to the folder where you want to save the notifications. This can be useful if you have multiple cameras connected to the same FTP server.
In the User and Password boxes, type the credentials for FTP access.
Click Apply.
To schedule actions, follow this procedure:
In the navigation pane, click Scheduler.
Click the check boxes to select which Scheduled actions to use.
In the schedule, click the Active check box for the days that the action will run:
Click Apply.
In the FTP Server box, type the IP address of the FTP server.
In the FTP User and FTP Password boxes, type the credentials for the FTP access.
Click Apply.
In the Recipient e-mail box, type the e-mail address of the recipient.
In the Mail server box, type the IP address of the sending mail server.
In the Sender e-mail box, type the e-mail address of the sender.
If the sending mail server requires a login (mail server authentication), select the Authenticate mail check box, and then type the credentials in the User and Password boxes.
Click Apply.
In the navigation pane, click MQTT.
Click the Enable MQTT check box.
Type the Broker host address and the TCP Broker Port used for the subscription transport.
Type the User and Password to login to the broker.
Select preferred Temperature unit in the list; Celsius (C), Fahrenheit (F), or Kelvin (K).
Select preferred Output format in the list; Json or Text.
Click Apply.
In your MQTT client of choice, set up a subscription for the topic corresponding to the information of interest. The topics will be updated when the data is updated, for example; if you subscribe to the topic FLIR/ec501-xxxxxx/alarm1, your MQTT client will receive an update when alarm1 is triggered and then another update when alarm1 criteria are no longer fulfilled. You can connect multiple cameras to the same MQTT broker.
In the navigation pane, click Modbus.
In the Digital out list, click Configure for the digital out number you want to use.
In the Digital output entry dialog box, type a Name of the entry. Also, type the IP Address, Device function ID, and Modbus Register address specific to the equipment.
Select Type specific to the equipment.
Click Apply.
To test the Modbus output, click Test which will activate the output for 5 seconds.
The digital out is now selectable in the Digital Out list when setting up alarms, see section 10.4.2 Working with alarms .
In the navigation pane, click Modbus.
In the Analogue out list, click Configure for the analogue out number you want to use.
In the Analogue output entry dialog box, type a Name of the entry.
Type the following information:
Click Apply.
To test the Modbus output, click Test which will activate the output for 5 seconds.
In the navigation pane, click Images.
To display a preview of an image, click the thumbnail of the image.
As an alternative, click the image file name, and then click Preview.
To download an image, click the image file name, and then click Download.
To delete one or more images, click the image file name(s), and then click Delete.
In the navigation pane, click Videos.
To download a video, click the video file name, and then click Download.
To delete one or more videos, click the video file name(s), and then click Delete.
In the navigation pane, click Logs.
To enable logging of alarms, click the Logging enabled check box.
To download the generated logs as a zipped file, click Download log.
To delete the generated logs, click Clean log.