13.1 FLIR Screen-EST software update
By default, a check for updates is performed automatically every time you start the FLIR Screen-EST application. You will be asked to install any available updates.
The settings for software updates are available on the
Updates tab, see section
10.3.6
Updates tab
.
Note
To check for and download updates, internet connection is required.
13.1.1 Offline update
If the FLIR EST Kiosk is not connected to the internet, you can update FLIR Screen-EST offline.
-
On a device with internet access, go to
https://support.flir.com/screenest
.
-
Download the FLIR Screen-EST installer package.
-
Transfer the installation package to the FLIR EST Kiosk tablet using e.g. a USB memory stick.
-
On the tablet, start the installation by double-clicking the executable installer file.
-
Read and accept the license terms and conditions.
-
Click Install.
-
Click Finish.
Note
To complete the installation, the tablet may need to be restarted. Follow the instructions on the screen.