1. Open the stand box and find the stand, foot, 2 screws, and Allen key. The other parts are not needed for this installation.
|
|
2. Mount the foot. Make sure the orientation of the foot is correct.
|
|
3. Check the orientation of the foot. Incorrect mounting can cause the stand to tip over.
|
4. Fit the tablet in place, with the clamp close to the buttons. By that, there will be room for the camera unit.
|
5. Rotate the tablet to portrait mode. Make sure the USB connector is at the bottom.
|
6. Slide the camera unit onto the stand.
|
7. Tilt the assembly backwards until it stops.
|
8. Lock the camera unit in place.
Tighten the screw until it stops. |
9. Connect the cable from the camera unit to the USB connector on the tablet.
|
10. Connect the power cable to the camera unit.
|
11. Connect the power cable to a power outlet.
|
12. Turn on the tablet.
|