7  Handling the camera

7.1  Charging the battery

7.1.1  General

  • Before starting the camera for the first time, charge the battery for 2 hours using the stand-alone battery charger.
  • Select a mains socket that is near the equipment and easily accessible.

7.1.2  Using the stand-alone battery charger to charge the battery

7.1.2.1  Stand-alone battery charger LED indicator

Type of signal

Explanation

The white LED flashes.
The battery is being charged.
The white LED glows continuously.
The battery is fully charged.

7.1.3  Using the USB battery charger to charge the battery

7.1.4  Charging the battery using a USB cable connected to a computer

7.2  Removing the battery

7.3  Turning on and turning off the camera

  • To turn on the camera, push the on/off button icon .
  • To turn off the camera, push and hold the on/off button icon for more than 0.5 second.

7.4  Adjusting the thermal camera focus

For accurate temperature measurements, it is very important to adjust the focus correctly.
You can adjust the camera focus by rotating the focus ring or by pushing the autofocus button. The camera can also be set up to perform continuous autofocusing.

7.4.1  Manual focus

To adjust the focus manually, rotate the focus ring.
Graphic

7.4.2  Autofocus

To autofocus the camera, push the Autofocus button.
Graphic

7.4.2.1  Autofocus method

When autofocusing, the camera can use one of the following focus methods:
  • Contrast: The focus is based on maximizing the image contrast.
  • Laser: The focus is based on a laser distance measurement. The laser is used when the camera is autofocusing.
The focus method is configured by a setting. Select icon (Settings) > Device settings > Focus > Auto focus and then select Contrast or Laser.

7.4.3  Continuous autofocus

The camera can be set up to perform continuous autofocusing.
When the continuous autofocus function is enabled, the camera bases the focus adjustments on continuous laser distance measurements. The laser is continuously on.
To enable or disable continuous autofocus, select icon (Settings) > Device settings > Focus > Continuous autofocus > On or Off.

7.5  P button

Graphic
The P button is used when screening in Operator mode.

You can also assign different functions to the programmable P button, by doing the following:

7.6  Remote operation button

The Remote operation button is used to trigger the screening in Button mode. The Remote operation button can also be used as an external P button in Operator mode.

7.6.1  Pair devices

Before you can use the Remote operation button with the camera, you need to pair the devices. See section 10.3.4.1 Pair with the button .

7.6.2  Change the battery

7.7  Zooming an image

You can zoom an image by using the camera’s digital zoom function. You can do this on live images and on saved images in edit mode.
To digitally zoom an image, do the following:
  • Zoom in: Touch the screen with two fingers and spread the fingers apart.
  • Zoom out: Touch the screen with two fingers and pinch the fingers together.

7.8  Connecting external devices and storage media

You can connect the following external devices and media to the camera:
  • An SD memory card.
  • A computer to move image and video files to and from the camera, using a USB-C to USB-A or a USB-C to USB-C cable.
  • A video monitor or projector, using a USB-C to HDMI adapter.
  • A USB battery charger.
Graphic

7.9  Configuring Wi-Fi

Depending on your camera configuration, you can connect the camera to a wireless local area network (WLAN) using Wi-Fi, or set up the camera as a wireless access point.

7.9.1  Connecting the camera to a WLAN

7.9.2  Setting up a wireless access point

7.10  Pairing Bluetooth‎ devices

You can use the camera with a Bluetooth-enabled headset.
Before you can use a Bluetooth device with the camera, you need to pair the devices.

Follow this procedure:

7.11  Operating the laser

The laser distance meter consists of a laser transmitter and a laser receiver. The laser distance meter determines the distance to a target by measuring the time it takes for a laser pulse to reach the target and return to the laser receiver. This time is converted to a distance, which is displayed on the screen.
The laser transmitter also works as a laser pointer. When the laser is on, you will see a laser dot approximately at the target.

To operate the laser, do the following:

7.12  Cleaning the camera

7.12.1  Camera housing, cables, and other items

    Use one of these liquids:
  • Warm water
  • A weak detergent solution
    Equipment:
  • A soft cloth

Follow this procedure:

7.12.2  Infrared lens

    Use one of these liquids:
  • A commercial lens cleaning liquid with more than 30% isopropyl alcohol.
  • 96% ethyl alcohol (C2H5OH).
    Equipment:
  • Cotton wool

Follow this procedure:

7.12.3  Infrared detector

Even small amounts of dust on the infrared detector can result in major blemishes in the image. To remove any dust from the detector, follow the procedure below.

7.13  Hand strap

The upper part of the hand strap is attached to the camera by a bracket. There is one bracket for the left side and one for the right side of the camera.
The lower part of the hand strap is threaded through the attachment point at the base of the camera.
Graphic

7.13.1  Mounting the hand strap

7.14  Lanyard strap

Graphic

7.15  Wrist strap

The wrist strap can also be used to attach a carabiner to the camera.
Graphic

7.16  Front protection

To protect the camera lens and the laser distance meter, you can attach the front protection by using the supplied fastening device.
Graphic

7.17  Changing camera lenses

Applicability: Camera models with an exchangeable lens.

7.18  Calibrating the lens–camera combination

Applicability: Camera models with an exchangeable lens.

7.18.1  Introduction

Before a new lens can be used with the camera, the lens–camera combination must be calibrated.
This is a process that previously had to be performed by a FLIR service department, but for the FLIR Exx-EST series the calibration can be performed by the user. This feature is called AutoCal. The AutoCal procedure requires a calibration target, which is included in the lens package.

7.18.2  AutoCal‎ procedure

To repeat the procedure at a later time, go to Settings > Camera information > Calibrate lens....

7.19  Calibrating the compass

It is recommended that the compass is calibrated every time you move the camera to a new location.

Follow this procedure: