11  Description — Screening station (Auto and Button mode)

This chapter describes a screening station for Auto mode or Button mode screening.

11.1  Overview

The screening station consists of a FLIR Exx-EST thermal camera, a clearly defined screening position, and a queueing system.
The thermal camera measures the temperature around the tear duct of the screened person, analyzes the measured temperature, and displays a screening result.
For improved measurement accuracy, it is important that the screened person is at the correct distance from the camera. The screening position indicates where the person should stand for the screening.
For an efficient screening flow, a queueing system is needed to guide the visitors into the screening station, to the correct screening position, and out of the screening station. A backdrop may be needed to prevent background disturbances from reaching the camera.

11.2  Typical setup

The figures below show a typical screening station setup.
Graphic
Graphic
    Additional, not in the figure:
  • Bluetooth button (Remote operation button).
    Used in Button mode to trigger the screening.
  • Optional: Operator display.
    Secondary display placed near the operator for monitoring.
  • Optional: Information roll-up.
    Roll-up that informs people what the screening is about and why they need to do it.
  • Optional: Instruction roll-up.
    Roll-up that tells people to remove eyeglasses before they are screened.

11.3  Screening station considerations

For accurate screening results and an efficient screening flow, the following factors related to the screening station area should be considered.
    Screening accuracy
  • Screening is best with room temperatures maintained below 24°C (76°F) and relative humidity below 50 %.
  • Screening should be carried out in an area with no air movement, out of direct sunlight, and away from heat sources.
  • Avoid locations with reflective backgrounds (e.g. windows, glass doors, or metallic surfaces).
    Equipment
  • The screening equipment is intended for indoor use.
  • Decide where the visitor display and the camera shall be placed and how they shall be mounted.
  • The screening equipment shall preferably be placed so that the operator can see the screening station and be of guidance to the screened persons.
  • It can be useful to have a secondary display for the operator, e.g. on the reception desk.
  • Power outlets are needed for the camera, computer, visitor display, and any operator display.
  • Avoid reflections in the visitor display. Otherwise, it can be difficult for the visitors to see the graphics and messages on the display.
    Visitors and queueing
  • Plan how the visitors will flow into the screening station and out, both in low and high flow periods. Plan for any alternative routes, e.g. after an alarm, for any questions, for persons in a wheelchair or with other special requirements.
  • Consider personal integrity matters; e.g. if the visitor display should be hidden from others than the screened person. See also section 11.4 Company policies .
  • Allow for appropriate distancing between people in the screening queue.
  • Allow for people to stabilize their temperature if it was raised by exercise or physical activity.

11.4  Company policies

The FLIR EST screening system only detects elevated skin temperatures. It is up to your company to set up a suitable screening process in accordance with applicable local data protection, employment, and health and safety laws.
    These are some of the factors your company need to consider:
  • Personal integrity
    Make decisions on how to handle personal integrity, e.g. show/hide the visitor display for others than the screened person, have/not have a sound alarm.
  • Process for alarms
    Establish a process for those individuals where the system has indicated an elevated temperature, e.g. let the person sit down for 10 minutes and then do the screening again, further evaluation by medically trained personnel.
  • Visitor information
    Provide visitors with information and instructions about the screening, e.g. by roll-ups.