4  Getting started

The FLIR Ignite functionality can be accessed as a web application through your browser and requires no installation. To get started, all you need to do is create a FLIR Ignite account. To upload images from your camera, you must also pair your camera with your FLIR Ignite account. For automatic syncing, you need to install FLIR Ignite Sync on your computer.

4.1  Accessing FLIR Ignite‎

You can access FLIR Ignite from a browser on your desktop, tablet, or mobile device.
To access FLIR Ignite, go to .

4.2  Creating an account

To create a FLIR Ignite account, go to and click Sign up.

4.3  Pairing

You start the pairing procedure from your FLIR Ignite enabled camera. The camera must be connected to a Wi-Fi network. You can do the pairing as part of the initial setup of the camera or at any time via the Settings menu in the camera. You will be guided through the pairing procedure by instructions on the camera screen. For more information, refer to the camera user manual.

4.4  Uploading images

Once the camera is paired with your FLIR Ignite account, you can upload images to your FLIR Ignite Library. You can set up the camera to automatically upload images when the camera is connected to a Wi-Fi network. You can also upload images manually from the camera. For more information, refer to the camera user manual.

4.5  Syncing

By installing FLIR Ignite Sync on your computer, you can automatically sync your FLIR Ignite Library with a sync folder on your computer. For more information, see chapter 8 FLIR Ignite Sync‎ .